MCUXpresso SDK Documentation

ZPS_tsAplZdpRecoverSourceBindReq

ZPS_tsAplZdpRecoverSourceBindReq#

This structure is used by the function ZPS_eAplZdpRecoverSourceBindRequest(). It represents a request to a remote node to recover the back-up of the local node’s source binding table (whole or in part).

The ZPS_tsAplZdpRecoverSourceBindReqstructure is detailed below.

typedef struct {
uint16 u16StartIndex;
} ZPS_tsAplZdpRecoverSourceBindReq;

where u16StartIndexis the binding table index of the first entry to be recovered.

Parent topic:ZDP Request structures