ZPS_tsAplZdpReplaceDeviceReq#
This structure is used by the function ZPS_eAplZdpReplaceDeviceRequest(). It represents a request to a remote node (with a primary binding table cache) to modify its binding table entries by replacing an IEEE address and/or associated endpoint number.
The ZPS_tsAplZdpReplaceDeviceReqstructure is detailed below.
typedef struct {
uint64 u64OldAddress; uint8 u8OldEndPoint; uint64 u64NewAddress; uint8 u8NewEndPoint;
} ZPS_tsAplZdpReplaceDeviceReq;
where:
u64OldAddressis the IEEE address to be replacedu8OldEndPointis the endpoint number to be replaced
(0-240, where 0 indicates that the endpoint number is not to be replaced)
u64NewAddressis the replacement IEEE addressu8NewEndPointis the replacement endpoint number (1-240)
Parent topic:ZDP Request structures