ZPS_tsAplZdpSimpleDescReq#
This structure is used by the function ZPS_eAplZdpSimpleDescRequest(). It represents a request for the Simple descriptor of an endpoint on the node with a given network address.
The ZPS_tsAplZdpSimpleDescReqstructure is detailed below.
typedef struct {
uint16 u16NwkAddrOfInterest;
uint8 u8EndPoint;
} ZPS_tsAplZdpSimpleDescReq;
where:
u16NwkAddrOfInterestis the network address of the node of interest.u8EndPointis the number of the relevant endpoint on the node (1-240).
Parent topic:ZDP Request structures