MCUXpresso SDK Documentation

ZPS_tsAplZdpSimpleDescStoreReq

ZPS_tsAplZdpSimpleDescStoreReq#

This structure is used by the function ZPS_eAplZdpSimpleDescStoreRequest(). It represents a request to a remote node to store the Simple descriptor of one of the local node’s endpoints.

The ZPS_tsAplZdpSimpleDescStoreReqstructure is detailed below.

typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr; uint8 u8Length;

/* Rest of message is variable length */ ZPS_tsAplZdpSimpleDescType sSimpleDescriptor;

} ZPS_tsAplZdpSimpleDescStoreReq;

where:

  • u16NwkAddris the network address of the sending node

  • u64IeeeAddris the IEEE address of the sending node

  • u8Lengthis the length of the Simple descriptor to store

  • sSimpleDescriptoris a pointer to the Simple descriptor to store (this is itself a structure of the type ZPS_tsAplZdpSimpleDescType, detailed in Section8.2.1.3)

Parent topic:ZDP Request structures