ZPS_tsAplZdpStoreBkupBindEntryReq#
This structure is used by the function ZPS_eAplZdpStoreBkupBindEntryRequest(). It represents a request to a remote node to save a back-up of an entry from the local primary binding table cache.
The ZPS_tsAplZdpStoreBkupBindEntryReqstructure is detailed below.
typedef struct {
uint64 u64SrcAddress;
uint8 u8SrcEndPoint;
uint16 u16ClusterId;
uint8 u8DstAddrMode;
union {
struct {
uint16 u16DstAddress;
} sShort;
struct {
uint64 u64DstAddress;
uint8 u8DstEndPoint;
} sExtended;
};
} ZPS_tsAplZdpStoreBkupBindEntryReq;
where:
u64SrcAddressis the IEEE address of the source node for the binding entryu8SrcEndpointis the number of the source endpoint for the binding (1-240)u16ClusterIdis the ID of the cluster (on the local endpoint) for the bindingu8DstAddrModeis the destination addressing mode for remaining elements (see Table 15 below)u16DstAddressis the address of the destination node for the binding (address type according to setting ofu8DstAddrMode)u8DstEndPointis the number of the destination endpoint for the binding (1-240)
Addressing modes
u8DstAddrMode |
Code |
Description |
|---|---|---|
0x01 |
ZPS_E_ADDR_MODE_GROUP |
16-bit Group address |
0x03 |
ZPS_E_ADDR_MODE_IEEE |
64-bit IEEE/MAC address |
Parent topic:ZDP Request structures