MCUXpresso SDK Documentation

ZPS_vExtendedStatusSetCallback

ZPS_vExtendedStatusSetCallback#

void ZPS_vExtendedStatusSetCallback(
   tpfExtendedStatusCallBack pfExtendedStatusCallBack);

Description#

This function can be used to register a callback function for extended error handling (see (Section 6.7)

The prototype of the callback function is:

ZPS_teExtendedStatus vExtendedStatusCb();

The registered callback function is invoked if a subsequent API function call results in one of the following errors:

  • 0xA3: ZPS_APL_APS_E_ILLEGAL_REQUEST

  • 0xA6: ZPS_APL_APS_E_INVALID_PARAMETER

  • 0xC2: ZPS_NWK_ENUM_INVALID_REQUEST

The callback function returns another error code (from those listed and described in Section 11.2.5), which provides a more specific reason for the error.

Parent topic:ZPS_vExtendedStatusSetCallback

Parameters#

pfExtendedStatusCallBackPointer to extended error handling callback function to be registered.

Parent topic:ZPS_vExtendedStatusSetCallback

Returns#

None.

Parent topic:ZPS_vExtendedStatusSetCallback

Parent topic:ZPS_vAplAfEnableMcpsFilter

Parent topic:initialization functions