BDB_tuBdbEventData

The following structure is a union containing the data for a ZigBee Base Device event.

typedef union
{
BDB_tsZpsAfEvent sZpsAfEvent;
BDB_tsFindAndBindEvent *psFindAndBindEvent;
}BDB_tuBdbEventData

where:

  • sZpsAfEvent is a structure containing the data for a stack event, indicated by the event type BDB_EVENT_ZPSAF - for a description of this structure, refer to Section 2.7.3.

  • psFindAndBindEvent is a pointer to a structure containing the data for a ‘Finding and Binding’ event (see Section 2.9) - for a description of this structure, refer to Section 2.7.4.

Parent topic:Structures