BDB_vSetKeys#
void BDB_vSetKeys(void);
Description#
This function loads into memory the appropriate pre-configured link key on the local node for the initial security state of the node. The function is automatically called by BDB_vInit(). However, it must be called explicitly to restore the link keys after a reset which removes the keys from memory.
The type of link key that is loaded depends on the node type, as follows:
On a Coordinator, the Default Global Trust Centre Link Key is loaded for participation in a centralized security network.
On a Router or End Device, both of the following keys are loaded:
Default Global Trust Centre Link Key for participation in a centralized security network.
Distributed Security Global Link Key for participation in a distributed security network.
The pre-configured link keys are defined in the file bdb_link_keys.c, from where they are loaded.
Network security is described in Section 2.3.
Parameters#
None
Returns#
None
Parent topic:Functions