Compile-time Options
To enable the Groups cluster in the code to be built, it is necessary to add the following to the zcl_options.h file:
#define CLD_GROUPS
In addition, to include the software for a cluster client or server or both, it is necessary to add one or both of the following to the same file:
#define GROUPS_CLIENT
#define GROUPS_SERVER
The Groups cluster contains macros that may be optionally specified at compile time by adding one or both of the following lines to the zcl_options.h file.
To set the size used for the group addressing table in the .zpscfg file,
Add this line:
#define CLD_GROUPS_MAX_NUMBER_OF_GROUPS             (8)
To configure the maximum length of the group name, add the following line:
#define CLD_GROUPS_MAX_GROUP_NAME_LENGTH            (16)
To define the value (n) of the Cluster Revision attribute, add the following line:
#define CLD_GROUPS_CLUSTER_REVISION <n>
The default value is 1, which corresponds to the revision of the cluster in the ZCL r6 specification (see Section 2.4).
Parent topic:Groups Cluster