Groups Cluster#
This chapter describes the Groups cluster which allows the management of the Group table concerned with group addressing.
The Groups cluster has a Cluster ID of 0x0004.
Overview#
The Groups cluster allows the management of group addressing that is available in ZigBee PRO. In this addressing scheme, an endpoint on a device can be a member of a group comprising endpoints from one or more devices. The group is assigned a 16-bit group ID or address. The group ID and the local member endpoint numbers are held in an entry of the Group table on a device. If a message is sent to a group address, the Group table is used to determine to which endpoints (if any) the message should deliver on the device. A group can be assigned a name of up to 16 characters and the cluster allows the support of group names to be enabled/disabled.
To use the functionality of this cluster, you must include the file Groups.h in your application and enable the cluster by defining CLD_GROUPS in the zcl_options.h file.
It is also necessary to enable the cluster as a server or client, or as both:
The cluster server is able to receive commands to modify the local group table.
The cluster client is able to send commands to the server to request changes to the group table on the server.
The inclusion of the client or server software must be pre-defined in the compile-time options of the application. In addition, if the cluster is to reside on a custom endpoint then the role of client or server must also be specified when creating the cluster instance.
The compile-time options for the Groups cluster are fully detailed in Section 12.8.
Parent topic:Groups Cluster
Groups Cluster structure and attributes#
The structure definition for the Groups cluster is:
typedef struct
{
zbmap8 u8NameSupport;
zuint16 u16ClusterRevision;
} tsCLD_Groups;
where:
u8NameSupportindicates whether group names are supported by the cluster:A most significant bit of 1 indicates that group names are supported.
A most significant bit of 0 indicates that group names are not supported.
u16ClusterRevisionis a mandatory attribute that specifies the revision of the cluster specification on which this cluster instance is based. The cluster specification in the ZCL r6 corresponds to a cluster revision of 1. The value is incremented by one for each subsequent revision of the cluster specification. This attribute is also described in Section 2.4.
Parent topic:Groups Cluster
Initialization#
The function eCLD_GroupsCreateGroups() is used to create an instance of the Groups cluster. The function is called by the initialization function for the host device.
A local endpoint can be added to a group on the local node using the function eCLD_GroupsAdd(). If the group does not exist, the function creates it. Therefore, this is a way of creating a local group.
Parent topic:Groups Cluster
Sending Commands#
The NXP implementation of the ZCL provides functions for sending commands between a Groups cluster client and server. A command is sent from the client to one or more endpoints on the server. Multiple endpoints can be targeted using binding or group addressing.
Adding Endpoints to Groups#
Two functions are provided for adding one or more endpoints to a group on a remote device. Each function sends a command to the endpoints to be added to the group, where the required group is specified in the payload of the command. If the group does not exist in the Group table of the target device, it is added to the table.
eCLD_GroupsCommandAddGroupRequestSend() can be used to request the addition of the target endpoints to the specified group.
eCLD_GroupsCommandAddGroupIfIdentifyingRequestSend() can be used to request the addition of the target endpoints to the specified group if the target device is in identification mode of the Identity cluster (see Chapter 11).
An endpoint can also be added to a local group, as described in Section 12.3.
Parent topic:Sending Commands
Removing Endpoints from Groups#
Two functions are provided for removing one or more endpoints from groups on a remote device. Each function sends a command to the endpoints to be removed from the groups. If a group is empty following the removal of the endpoint, it is deleted in the Group table.
eCLD_GroupsCommandRemoveGroupRequestSend() can be used to request the removal of the target endpoint from the group which is specified in the payload of the command.
eCLD_GroupsCommandRemoveAllGroupsRequestSend() can be used to request the removal of the target endpoint from all groups on the remote device.
If an endpoint is a member of a scene associated with a group to be removed, the above function calls also results in the removal of the endpoint from the scene.
Parent topic:Sending Commands
Obtaining Information about Groups#
Two functions are provided for obtaining information about groups. Each function sends a command to the endpoints to which the inquiry relates.
eCLD_GroupsCommandViewGroupRequestSend() can be used to request the name of a group with the ID/address specified in the command payload.
eCLD_GroupsCommandGetGroupMembershipRequestSend() can be used to determine whether the target endpoint is a member of any of the groups specified in the command payload.
Parent topic:Sending Commands
Parent topic:Groups Cluster
Functions#
The following Groups cluster functions are provided in the NXP implementation of the ZCL:
eCLD_GroupsCreateGroups#
teZCL_Status eCLD_GroupsCreateGroups(
tsZCL_ClusterInstance *psClusterInstance,
bool_t bIsServer,
tsZCL_ClusterDefinition *psClusterDefinition,
void *pvEndPointSharedStructPtr,
tsCLD_GroupsCustomDataStructure
*psCustomDataStructure,
tsZCL_EndPointDefinition *psEndPointDefinition);
Description#
This function creates an instance of the Groups cluster on an endpoint. The cluster instance is created on the endpoint which is associated with the supplied tsZCL_ClusterInstance structure and can act as a server or a client, as specified.
The function must be called when setting up a custom endpoint containing one or more selected clusters (rather than the whole set of clusters supported by a standard ZigBee device). This function creates a Groups cluster instance on the endpoint, but instances of other clusters may also be created on the same endpoint by calling their corresponding creation functions.
Note: Do not call this function for an endpoint on which a standard ZigBee device is used. In this case, the device and its supported clusters must be registered on the endpoint using the relevant device registration function.
When used, this function must be the first Groups cluster function called in the application, and must be called after the stack has been started and after the ZCL has been initialized.
The function retrieves any group IDs already stored in the Application Information Base (AIB) of the ZigBee PRO stack. However, the AIB does not store group names. If name support is required, the application should store the group names using the NVM module, so that they can be retrieved following a power outage.
Parameters#
psClusterInstance: Pointer to structure containing information about the cluster instance to be created (see Section 6.1.16). This structure is updated by the function by initializing individual structure fields.
bIsServer: Type of cluster instance (server or client) to be created:
TRUE - server
FALSE - client
psClusterDefinition: Pointer to structure indicating the type of cluster to be created (see Section 6.1.2). In this case, this structure must contain the details of the Groups cluster. This parameter can refer to a pre-filled structure called
sCLD_Groupswhich is provided in the Groups.h file.pvEndPointSharedStructPtr: Pointer to the shared structure used for attribute storage. This parameter should be the address of the structure of type
tsCLD_Groupswhich defines the attributes of Groups cluster. The function initializes the attributes with default values.psCustomDataStructure: Pointer to a structure containing the storage for internal functions of the cluster (see [Section 12.6.1](custom_data_structure.md #id_1d50fd17-874c-48c4-b748-e26925fd08d3)).
psEndPointDefinition: Pointer to the ZCL endpoint definition structure for the application (see Section 6.1.1).
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
Parent topic:Functions
eCLD_GroupsAdd#
teZCL_Status eCLD_GroupsAdd(uint8 u8SourceEndPointId,
uint16 u16GroupId,
uint8 *pu8GroupName);
Description#
This function adds the specified endpoint on the local node to the group with the specified group ID/address and specified group name. The relevant entry is modified in the Group table on the local endpoint (of the calling application). If the group does not currently exist, it is created by adding a new entry for the group to the Group table.
Note that the number of entries in the Group table must not exceed the value of CLD_GROUPS_MAX_NUMBER_OF_GROUPS defined at compile time (see Section 12.8).
Parameters#
u8SourceEndPointId: Number of local endpoint to be added to group.
u16GroupId: 16-bit group ID/address of group.
pu8GroupName: Pointer to character string representing name of group.
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions
eCLD_GroupsCommandAddGroupRequestSend#
teZCL_Status eCLD_GroupsCommandAddGroupRequestSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_Groups_AddGroupRequestPayload
*psPayload);
Description#
This function sends an Add Group command to a remote device, requesting that the specified endpoints on the target device be added to a group. The group ID/address and name (if supported) are specified in the payload of the message, and must be added to the Group table on the target node along with the associated endpoint numbers.
The device receiving this message generates a callback event on the endpoint on which the Groups cluster is registered. Also, add the group to its Group table before sending a response indicating success or failure (see Section 12.6.4).
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters#
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.
psPayload: Pointer to a structure containing the payload for this message (see Section 12.6.3).
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions
eCLD_GroupsCommandViewGroupRequestSend#
teZCL_Status eCLD_GroupsCommandViewGroupRequestSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_Groups_ViewGroupRequestPayload
*psPayload);
Description#
This function sends a View Group command to a remote device, requesting the name of the group with the specified group ID (address) on the destination endpoint.
The device receiving this message generates a callback event on the endpoint on which the Groups cluster was registered and generates a View Group response containing the group name (see Section 12.6.4).
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters#
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.
psPayload: Pointer to a structure containing the payload for this message (see Section 12.6.3).
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions
eCLD_GroupsCommandGetGroupMembershipRequestSend#
teZCL_Status eCLD_GroupsCommandGetGroupMembershipRequestSend
(uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_Groups_GetGroupMembershipRequestPayload
*psPayload);
Description#
This function sends a Get Group Membership command to inquire whether the target endpoint is a member of any of the groups specified in a list contained in the command payload.
The device receiving this message generates a callback event on the endpoint on which the Groups cluster is registered and generates a Get Group Membership response containing the required information (see Section 12.6.4).
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters#
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.
psPayload: Pointer to a structure containing the payload for this message (see Section 12.6.3).
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions
eCLD_GroupsCommandRemoveGroupRequestSend#
teZCL_Status eCLD_GroupsCommandRemoveGroupRequestSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_Groups_RemoveGroupRequestPayload
*psPayload);
Description#
This function sends a Remove Group command to request that the target device deletes membership of the destination endpoints from a particular group - that is, remove the endpoints from the entry of the group in the Group table on the device and, if no other endpoints remain in the group, remove the group from the table.
The device receiving this message generates a callback event on the endpoint on which the Groups cluster is registered. If the group becomes empty following the deletion, the device removes the group ID and group name from its Group table. It then generates an appropriate Remove Group response indicating success or failure (see Section 12.6.4).
If the target endpoint belongs to a scene associated with the group to be removed (requiring the Scenes cluster - see Chapter 13), the endpoint is also removed from this scene as a result of this function call - that is, the relevant scene entry is deleted from the Scene table on the target device.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters#
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.
u8DestinationEndPointId: The number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.
psPayload: Pointer to a structure containing the payload for this message (see Section 12.6.3).
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions
eCLD_GroupsCommandRemoveAllGroupsRequestSend#
teZCL_Status eCLD_GroupsCommandRemoveAllGroupsRequestSend
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber);
Description#
This function sends a Remove All Groups command to request that the target device removes all group memberships of the destination endpoints. Issuing this command removes the endpoints from all group entries in the Group table on the device. If no other endpoints remain in a group, the function removes the group from the table.
The device receiving this message generates a callback event on the endpoint on which the Groups cluster is registered. If a group becomes empty following the deletion, the device removes the group ID and group name from its Group table.
If the target endpoint belongs to scenes associated with the groups to be removed, calling this function also removes the endpoint from the scenes. The relevant scene entries are deleted from the Scene table on the target device. (For details about the Scenes cluster - refer to Chapter 13).
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters#
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.
u8DestinationEndPointId: The number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
The eCLD_GroupsCommandRemoveAllGroupsRequestSend function invokes the ZigBee PRO stack function to transmit the data. If the ZigBee PRO stack function returns an error, the same can be obtained by calling the eZCL_GetLastZpsError() function.
Parent topic:Functions
eCLD_GroupsCommandAddGroupIfIdentifyingRequestSend#
teZCL_Status eCLD_GroupsCommandAddGroupIfIdentifyingRequestSend
(uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_Groups_AddGroupRequestPayload
*psPayload);
Description#
This function sends an Add Group If Identifying command to a remote device, requesting that the specified endpoints on the target device be added to a particular group on the condition that the remote device is identifying itself. The group ID/address and name (if supported) are specified in the payload of the message, and must be added to the Group table on the target node along with the associated endpoint numbers. The identifying functionality is controlled using the Identify cluster (see Chapter 11).
The device receiving this message generates a callback event on the endpoint on which the Groups cluster is registered and then checks whether the device is identifying itself. If so, the device (if possible) adds the group ID and group name to its Group table. If the device is not identifying itself, then no action is taken.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters#
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.
psPayload: Pointer to a structure containing the payload for this message (see Section 12.6.3).
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function, which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions
Parent topic:Groups Cluster
Structures#
Custom Data Structure#
The Groups cluster requires extra storage space to be allocated to be used by internal functions. The structure definition for this storage is shown below:
typedef struct
{
DLIST lGroupsAllocList;
DLIST lGroupsDeAllocList;
bool bIdentifying;
tsZCL_ReceiveEventAddress sReceiveEventAddress;
tsZCL_CallBackEvent sCustomCallBackEvent;
tsCLD_GroupsCallBackMessage sCallBackMessage;
#if (defined CLD_GROUPS) && (defined GROUPS_SERVER)
tsCLD_GroupTableEntry
asGroupTableEntry[CLD_GROUPS_MAX_NUMBER_OF_GROUPS];
#endif
} tsCLD_GroupsCustomDataStructure;
The fields are for internal use and no knowledge of them is required.
However, the structure tsCLD_GroupTableEntry used for the Group table entries is shown in Section 12.6.2.
Parent topic:Structures
Group Table Entry#
The following structure contains a Group table entry.
typedef struct
{
DNODE dllGroupNode;
uint16 u16GroupId;
uint8 au8GroupName[CLD_GROUPS_MAX_GROUP_NAME_LENGTH + 1];
} tsCLD_GroupTableEntry;
The fields are for internal use and no knowledge of them is required.
Parent topic:Structures
Custom Command Payloads#
The following structures contain the payloads for the Groups cluster custom commands.
Add Group Request Payload#
typedef struct
{
zuint16 u16GroupId;
tsZCL_CharacterString sGroupName;
} tsCLD_Groups_AddGroupRequestPayload;
where:
u16GroupIdis the ID/address of the group to which the endpoints must be added.sGroupNameis the name of the group to which the endpoints must be added.
View Group Request Payload#
typedef struct
{
zuint16 u16GroupId;
} tsCLD_Groups_ViewGroupRequestPayload;
where u16GroupId is the ID/address of the group whose name is required
Get Group Membership Request Payload#
typedef struct
{
zuint8 u8GroupCount;
zint16 *pi16GroupList;
} tsCLD_Groups_GetGroupMembershipRequestPayload;
where:
u8GroupCountis the number of groups in the list of the next field.pi16GroupListis a pointer to a list of groups whose memberships are being queried, where each group is represented by its group ID/address.
Remove Group Request Payload#
typedef struct
{
zuint16 u16GroupId;
} tsCLD_Groups_RemoveGroupRequestPayload;
where u16GroupId is the ID/address of the group from which the endpoints must be removed.
Parent topic:Structures
Custom Command Responses#
The Groups cluster generates responses to certain custom commands. The responses which contain payloads are detailed below:
Add Group Response Payload#
typedef struct
{
zenum8 eStatus;
zuint16 u16GroupId;
} tsCLD_Groups_AddGroupResponsePayload;
where:
eStatusis the status (success or failure) of the requested group addition.u16GroupIdis the ID/address of the group to which endpoints were added.
View Group Response Payload#
typedef struct
{
zenum8 eStatus;
zuint16 u16GroupId;
tsZCL_CharacterString sGroupName;
} tsCLD_Groups_ViewGroupResponsePayload;
where:
eStatusis the status (success or failure) of the requested operation.u16GroupIdis the ID/address of the group whose name was requested.sGroupNameis the returned name of the specified group.
Get Group Membership Response Payload#
typedef struct
{
zuint8 u8Capacity;
zuint8 u8GroupCount;
zint16 *pi16GroupList;
} tsCLD_Groups_GetGroupMembershipResponsePayload;
where:
u8Capacityis the capacity of the Group table of the device to receive more groups - that is, the number of groups that may be added (special values: 0xFE means that at least one additional group may be added, a higher value means that the remaining capacity of the table is unknown).u8GroupCountis the number of groups in the list of the next field.pi16GroupListis a pointer to the returned list of groups from those queried that exist on the device, where each group is represented by its group ID/address.
Remove Group Response Payload#
typedef struct
{
zenum8 eStatus;
zuint16 u16GroupId;
} tsCLD_Groups_RemoveGroupResponsePayload;
where:
eStatusis the status (success or failure) of the requested group modification.u16GroupIdis the ID/address of the group from which endpoints were removed.
Parent topic:Structures
Parent topic:Groups Cluster
Enumerations#
teCLD_Groups_ClusterID#
The following structure contains the enumeration used to identify the attribute of the Groups cluster.
typedef enum
{
E_CLD_GROUPS_ATTR_ID_NAME_SUPPORT = 0x0000 /* Mandatory */
} teCLD_Groups_ClusterID;
Parent topic:Enumerations
Parent topic:Groups Cluster
Compile-time Options#
To enable the Groups cluster in the code to be built, it is necessary to add the following to the zcl_options.h file:
#define CLD_GROUPS
In addition, to include the software for a cluster client or server or both, it is necessary to add one or both of the following to the same file:
#define GROUPS_CLIENT
#define GROUPS_SERVER
The Groups cluster contains macros that may be optionally specified at compile time by adding one or both of the following lines to the zcl_options.h file.
To set the size used for the group addressing table in the .zpscfg file,
Add this line:
#define CLD_GROUPS_MAX_NUMBER_OF_GROUPS (8)
To configure the maximum length of the group name, add the following line:
#define CLD_GROUPS_MAX_GROUP_NAME_LENGTH (16)
To define the value (n) of the Cluster Revision attribute, add the following line:
#define CLD_GROUPS_CLUSTER_REVISION <n>
The default value is 1, which corresponds to the revision of the cluster in the ZCL r6 specification (see Section 2.4).
Parent topic:Groups Cluster