MCUXpresso SDK Documentation

Custom Command Responses#

The Groups cluster generates responses to certain custom commands. The responses which contain payloads are detailed below:

Add Group Response Payload#

typedef struct
{
    zenum8            eStatus;
    zuint16            u16GroupId;
} tsCLD_Groups_AddGroupResponsePayload;

where:

  • eStatus is the status (success or failure) of the requested group addition.

  • u16GroupId is the ID/address of the group to which endpoints were added.

View Group Response Payload#

typedef struct
{
    zenum8                  eStatus;
    zuint16                 u16GroupId;
    tsZCL_CharacterString   sGroupName;
} tsCLD_Groups_ViewGroupResponsePayload;

where:

  • eStatus is the status (success or failure) of the requested operation.

  • u16GroupId is the ID/address of the group whose name was requested.

  • sGroupName is the returned name of the specified group.

Get Group Membership Response Payload#

typedef struct
{
    zuint8                  u8Capacity;
    zuint8                  u8GroupCount;
    zint16                 *pi16GroupList;
} tsCLD_Groups_GetGroupMembershipResponsePayload;

where:

  • u8Capacity is the capacity of the Group table of the device to receive more groups - that is, the number of groups that may be added (special values: 0xFE means that at least one additional group may be added, a higher value means that the remaining capacity of the table is unknown).

  • u8GroupCount is the number of groups in the list of the next field.

  • pi16GroupList is a pointer to the returned list of groups from those queried that exist on the device, where each group is represented by its group ID/address.

Remove Group Response Payload#

typedef struct
{
    zenum8               eStatus;
    zuint16              u16GroupId;
} tsCLD_Groups_RemoveGroupResponsePayload;

where:

  • eStatus is the status (success or failure) of the requested group modification.

  • u16GroupId is the ID/address of the group from which endpoints were removed.

Parent topic:Structures