Structures#
Custom Data Structure#
The Groups cluster requires extra storage space to be allocated to be used by internal functions. The structure definition for this storage is shown below:
typedef struct
{
DLIST lGroupsAllocList;
DLIST lGroupsDeAllocList;
bool bIdentifying;
tsZCL_ReceiveEventAddress sReceiveEventAddress;
tsZCL_CallBackEvent sCustomCallBackEvent;
tsCLD_GroupsCallBackMessage sCallBackMessage;
#if (defined CLD_GROUPS) && (defined GROUPS_SERVER)
tsCLD_GroupTableEntry
asGroupTableEntry[CLD_GROUPS_MAX_NUMBER_OF_GROUPS];
#endif
} tsCLD_GroupsCustomDataStructure;
The fields are for internal use and no knowledge of them is required.
However, the structure tsCLD_GroupTableEntry used for the Group table entries is shown in Section 12.6.2.
Parent topic:Structures
Group Table Entry#
The following structure contains a Group table entry.
typedef struct
{
DNODE dllGroupNode;
uint16 u16GroupId;
uint8 au8GroupName[CLD_GROUPS_MAX_GROUP_NAME_LENGTH + 1];
} tsCLD_GroupTableEntry;
The fields are for internal use and no knowledge of them is required.
Parent topic:Structures
Custom Command Payloads#
The following structures contain the payloads for the Groups cluster custom commands.
Add Group Request Payload#
typedef struct
{
zuint16 u16GroupId;
tsZCL_CharacterString sGroupName;
} tsCLD_Groups_AddGroupRequestPayload;
where:
u16GroupIdis the ID/address of the group to which the endpoints must be added.sGroupNameis the name of the group to which the endpoints must be added.
View Group Request Payload#
typedef struct
{
zuint16 u16GroupId;
} tsCLD_Groups_ViewGroupRequestPayload;
where u16GroupId is the ID/address of the group whose name is required
Get Group Membership Request Payload#
typedef struct
{
zuint8 u8GroupCount;
zint16 *pi16GroupList;
} tsCLD_Groups_GetGroupMembershipRequestPayload;
where:
u8GroupCountis the number of groups in the list of the next field.pi16GroupListis a pointer to a list of groups whose memberships are being queried, where each group is represented by its group ID/address.
Remove Group Request Payload#
typedef struct
{
zuint16 u16GroupId;
} tsCLD_Groups_RemoveGroupRequestPayload;
where u16GroupId is the ID/address of the group from which the endpoints must be removed.
Parent topic:Structures
Custom Command Responses#
The Groups cluster generates responses to certain custom commands. The responses which contain payloads are detailed below:
Add Group Response Payload#
typedef struct
{
zenum8 eStatus;
zuint16 u16GroupId;
} tsCLD_Groups_AddGroupResponsePayload;
where:
eStatusis the status (success or failure) of the requested group addition.u16GroupIdis the ID/address of the group to which endpoints were added.
View Group Response Payload#
typedef struct
{
zenum8 eStatus;
zuint16 u16GroupId;
tsZCL_CharacterString sGroupName;
} tsCLD_Groups_ViewGroupResponsePayload;
where:
eStatusis the status (success or failure) of the requested operation.u16GroupIdis the ID/address of the group whose name was requested.sGroupNameis the returned name of the specified group.
Get Group Membership Response Payload#
typedef struct
{
zuint8 u8Capacity;
zuint8 u8GroupCount;
zint16 *pi16GroupList;
} tsCLD_Groups_GetGroupMembershipResponsePayload;
where:
u8Capacityis the capacity of the Group table of the device to receive more groups - that is, the number of groups that may be added (special values: 0xFE means that at least one additional group may be added, a higher value means that the remaining capacity of the table is unknown).u8GroupCountis the number of groups in the list of the next field.pi16GroupListis a pointer to the returned list of groups from those queried that exist on the device, where each group is represented by its group ID/address.
Remove Group Response Payload#
typedef struct
{
zenum8 eStatus;
zuint16 u16GroupId;
} tsCLD_Groups_RemoveGroupResponsePayload;
where:
eStatusis the status (success or failure) of the requested group modification.u16GroupIdis the ID/address of the group from which endpoints were removed.
Parent topic:Structures
Parent topic:Groups Cluster