MCUXpresso SDK Documentation

Initialization

Initialization#

The function         eCLD_GroupsCreateGroups() is used to create an instance of the Groups cluster. The function is called by the initialization function for the host device.

A local endpoint can be added to a group on the local node using the function eCLD_GroupsAdd(). If the group does not exist, the function creates it. Therefore, this is a way of creating a local group.

Parent topic:Groups Cluster