MCUXpresso SDK Documentation

eOTA_ClientQueryNextImageRequest

eOTA_ClientQueryNextImageRequest#

teZCL_Status eOTA_ClientQueryNextImageRequest(
    uint8 u8SourceEndpoint,
    uint8 u8DestinationEndpoint,
    tsZCL_Address *psDestinationAddress,
    tsOTA_QueryImageRequest
*psQueryImageRequest);

Description#

This function issues a Query Next Image Request to the server and should be called in either of the following situations:

  • to poll for a new application image (typically used in this way by an End Device) - in this case, the function should normally be called periodically

  • to respond to an Image Notify message from the server, which indicated that a new application image is available for download - in this case, the function call should be prompted by the event E_CLD_OTA_COMMAND_IMAGE_NOTIFY

The payload of the request includes the relevant image type, current file version, hardware version and manufacturer code.

As a result of this function call, a Query Next Image Response will (eventually) be received from the server. The arrival of this response will trigger an E_CLD_OTA_COMMAND_QUERY_NEXT_IMAGE_RESPONSE event.

Parameters#

  • u8SourceEndpoint: Number of endpoint (on client) from which the request is sent

  • u8DestinationEndpoint: Number of endpoint (on server) to which the request is sent

  • psDestinationAddress: Pointer to structure containing the address of the target server (see Section 6.1.4)

  • psQueryImageRequest: Pointer to structure containing payload for request (see Section 49.11.6)

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_FAIL

Parent topic:Client Functions