MCUXpresso SDK Documentation

tsOTA_QueryImageRequest

tsOTA_QueryImageRequest#

The following structure contains payload data for a Query Next Image Request issued by a client to poll the server for an upgrade image or to respond to an Image Notify message from the server:

typedef struct
{
    uint32 u32CurrentFileVersion;
    uint16 u16HardwareVersion;
    uint16 u16ImageType;
    uint16 u16ManufacturerCode;
    uint8  u8FieldControl;
}tsOTA_QueryImageRequest;

where:

  • u32CurrentFileVersion is the file version of the application image that is currently running on the client that sent the request

  • u16HardwareVersion is the hardware version of the client device (this information is optional - see u8FieldControl below)

  • u16ImageType is a value in the range 0x0000-0xFFBF which identifies the type of image currently running on the client

  • u16ManufacturerCode is the ZigBee-assigned number identifying the manufacturer of the client device

  • u8FieldControl is a bitmap indicating whether certain optional information about the client is included in this Query Next Image Request message. Currently, this optional information consists only of the hardware version (contained in u16HardwareVersion above) - bit 0 is set to ‘1’ if the hardware version is included or to ‘0’ otherwise (all other bits are reserved)

Parent topic:Structures