MCUXpresso SDK Documentation

eOTA_ServerQuerySpecificFileResponse

eOTA_ServerQuerySpecificFileResponse#

teZCL_Status eOTA_ServerQuerySpecificFileResponse(
    uint8 u8SourceEndpoint,
    uint8 u8DestinationEndpoint,
    tsZCL_Address *psDestinationAddress,
    tsOTA_QuerySpecificFileResponsePayload
    *psQuerySpecificFileResponsePayload,
    uint8 u8TransactionSequenceNumber);

Description#

This function can be used to issue a Query Specific File Response to a client which has sent a Query Specific File Request (the arrival of this request triggers the event E_CLD_OTA_COMMAND_QUERY_SPECIFIC_FILE_REQUEST on the server). The Query Specific File Response contains information on the latest device-specific file available for download to the client, including the file size and file version.

You are also required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters#

  • u8SourceEndpoint: Number of endpoint (on server) from which the response is sent

  • u8DestinationEndpoint: Number of endpoint (on client) to which the response is sent

  • psDestinationAddress: Pointer to structure containing the address of the target client

  • psQuerySpecificFileResponsePayload:

  • Pointer to structure containing payload for Query Specific File Response (see Section 49.11.20)

  • u8TransactionSequenceNumber: Pointer to a location to store the Transaction Sequence Number (TSN) of the request

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_FAIL

Parent topic:Server Functions