MCUXpresso SDK Documentation

tsOTA_QuerySpecificFileResponsePayload

tsOTA_QuerySpecificFileResponsePayload#

The following structure contains the payload for a Query Specific File Response which is issued by an OTA Upgrade server in response to a request for a device-specific file.

typedef struct
{
    uint32 u32FileVersion;
    uint32 u32ImageSize;
    uint16 u16ImageType;
    uint16 u16ManufacturerCode;
    uint8 u8Status;
}tsOTA_QuerySpecificFileResponsePayload;

where:

  • 32FileVersion contains the release and build numbers of the application and stack that correspond to the device-specific file - this field will take the same value as the equivalent field in the corresponding Query Specific File Request (see Section 49.11.19)

  • u32ImageSize is the size of the requested file, in bytes

  • u16ImageType indicates the requested file type - this field will take the same value as the equivalent field in the corresponding Query Specific File Request (see Section 49.11.19)

  • u16ManufactuerCode is the ZigBee-assigned manufacturer code of the requesting node - this field will take the same value as the equivalent field in the corresponding Query Specific File Request (see Section 49.11.19)

  • u8Status indicates whether a suitable file is available for download:

    • OTA_STATUS_SUCCESS: A suitable file is available

    • OTA_STATUS_NO_IMAGE_AVAILABLE: No suitable file is available

      • The other elements of the structure are only included in the case of success.

Parent topic:Structures