MCUXpresso SDK Documentation

tsOTA_Common

tsOTA_Common#

The following structure contains data relating to an OTA message received by the cluster (server or client) - this data is used for callback functions and the local OTA state machine:

typedef struct
{
    tsZCL_ReceiveEventAddress  sReceiveEventAddress;
    tsZCL_CallBackEvent        sOTACustomCallBackEvent;
    tsOTA_CallBackMessage      sOTACallBackMessage;
} tsOTA_Common;

The fields are for internal use and no knowledge of them is required. The tsOTA_CallBackMessage structure is described in Section 49.11.21.

Parent topic:Structures