Structures#
tsOTA_ImageHeader#
The following structure contains information for the OTA header:
typedef struct
{
uint32 u32FileIdentifier;
uint16 u16HeaderVersion;
uint16 u16HeaderLength;
uint16 u16HeaderControlField;
uint16 u16ManufacturerCode;
uint16 u16ImageType;
uint32 u32FileVersion;
uint16 u16StackVersion;
uint8 stHeaderString[OTA_HEADER_STRING_SIZE];
uint32 u32TotalImage;
uint8 u8SecurityCredVersion;
uint64 u64UpgradeFileDest;
uint16 u16MinimumHwVersion;
uint16 u16MaxHwVersion;
}tsOTA_ImageHeader;
where:
u32FileIdentifieris a 4-byte value equal to 0x0BEEF11E which indicates that the file contains an OTA upgrade imageu16HeaderVersionis the version of the OTA header expressed as a 2-byte value in which the most significant byte contains the major version number and the least significant byte contains the minor version numberu16HeaderLengthis the full length of the OTA header, in bytesu16HeaderControlFieldis a bitmap indicating certain information about the file, as detailed in table below.
Bit |
Information |
|---|---|
0 |
Security credential version (in OTA header): |
1: Field present in header
0: Field not present in header
|
|1|Device-specific file (also see u64UpgradeFileDest):
1: File is device-specific
0: File is not device-specific
| |2|Maximum and minimum hardware version (in OTA header):
1: Field present in header
0: Field not present in header
| |3-15|Reserved|
u16ManufacturerCodeis the ZigBee-assigned manufacturer code (0xFFFF is a wildcard value, representing any manufacturer)u16ImageTypeis a unique value representing the image type, where this value is normally manufacturer-specific but certain values have been reserved for specific file types, as indicated below (the wildcard value of 0xFFFF represents any file type):
Value |
File Type |
|---|---|
0x0000 – 0xFFBF |
Manufacturer-specific |
0xFFC0 |
Security credential |
0xFFC1 |
Configuration |
0xFFC2 |
Log |
0xFFC3 – 0xFFFE |
Reserved |
0xFFFF |
Wildcard |
u32FileVersioncontains the release and build numbers of the application and stack used to produce the application image - for details of the file version format, refer to the ZigBee Over-the-Air Upgrading Cluster Specification (095264)u16StackVersioncontains ZigBee stack version that is used by the application (this is 0x0002 for ZigBee PRO)stHeaderString[]is a manufacturer-specific string that can be used to store any useful human-readable informationu32TotalImageis the total size, in bytes, of the image that will be transferred over-the air (including the OTA header and any optional data)u8SecurityCredVersionindicates the security credential version type that is required by the client in order to install the image - the possibilities are SE1.0 (0x0), SE1.1 (0x1) and SE2.0 (0x2)u64UpgradeFileDestcontains the IEEE/MAC address of the destination device for the file, in the case when the file is device-specific (as indicated by bit 1 ofu16HeaderControlField)u16MinimumHwVersionindicates the earliest hardware platform on which the image should be used, expressed as a 2-byte value in which the most significant byte contains the hardware version number and the least significant byte contains the revision numberu16MaxHwVersionindicates the latest hardware platform on which the image should be used, expressed as a 2-byte value in which the most significant byte contains the hardware version number and the least significant byte contains the revision number
Parent topic:Structures
tsOTA_Common#
The following structure contains data relating to an OTA message received by the cluster (server or client) - this data is used for callback functions and the local OTA state machine:
typedef struct
{
tsZCL_ReceiveEventAddress sReceiveEventAddress;
tsZCL_CallBackEvent sOTACustomCallBackEvent;
tsOTA_CallBackMessage sOTACallBackMessage;
} tsOTA_Common;
The fields are for internal use and no knowledge of them is required. The tsOTA_CallBackMessage structure is described in Section 49.11.21.
Parent topic:Structures
tsOTA_HwFncTable#
The following structure contains pointers to callback functions to be used by the OTA Upgrade cluster to perform initialization, erase, write and read operations on Flash memory (if these functions are not specified, standard NXP functions will be used):
typedef struct
{
void (*prInitHwCb)(uint8, void*);
void (*prEraseCb) (uint8 u8Sector);
void (*prWriteCb) (uint32 u32FlashByteLocation,
uint16 u16Len,
uint8 *pu8Data);
void (*prReadCb) (uint32 u32FlashByteLocation,
uint16 u16Len,
uint8 *pu8Data);
} tsOTA_HwFncTable;
where:
prInitHwCbis a pointer to a callback function that is called after a cold or warm start to perform any initialization required for the Flash memory deviceprEraseCbis a pointer to a callback function that is called to erase a specified sector of Flash memoryprWriteCbis a pointer to a callback function that is called to write a block of data to a sector, starting the write at a specified byte location in the sector (address zero is the start of the sector)prReadCbis a pointer to a callback function that is called to read a block of data from a sector, starting the read at a specified byte location in the sector (address zero is the start of the sector)
Parent topic:Structures
tsNvmDefs#
The following structure contains information used to configure access to Flash memory:
typedef struct
{
tsOTA_HwFncTable sOtaFnTable;
uint32 u32SectorSize;
uint8 u8FlashDeviceType;
}tsNvmDefs;
where:
sOtaFnTableis a structure specifying the callback functions to be used by the cluster to perform initialization, erase, write and read operations on the Flash memory device (see Section 49.11.3) - if user-defined callback functions are not specified, standard NXP functions will be usedu32SectorSizeis the size of a sector of the Flash memory device, in bytesu8FlashDeviceTypeis a value indicating the type of Flash memory device, one of:E_FL_CHIP_INTERNAL (Device internal Flash- default)
Parent topic:Structures
tsOTA_ImageNotifyCommand#
The following structure contains the payload data for an Image Notify message issued by the server when a new upgrade image is available for download:
typedef struct
{
teOTA_ImageNotifyPayloadType ePayloadType;
uint32 u32NewFileVersion;
uint16 u16ImageType;
uint16 u16ManufacturerCode;
uint8 u8QueryJitter;
}tsOTA_ImageNotifyCommand;
where:
ePayloadTypeis a value indicating the type of payload of the command (enumerations are available - see Section 49.12.4)u32NewFileVersionis the file version of the client upgrade image that is currently available for download (the wild card of 0xFFFFFFFF is used to indicate that all clients should upgrade to this image)u16ImageTypeis a number indicating the type of image that is available for download (the wild card of 0xFFFF is used to indicate that all image types are involved)u16ManufacturerCodeis a ZigBee-assigned number identifying the manufacturer to which the available image is connected (if all manufacturers are involved, this value should not be set)u8QueryJitteris a value between 1 and 100 (inclusive) which is used by the receiving client to decide whether to reply to this Image Notify message - for information on ‘Query Jitter’, refer to Section 49.7
Parent topic:Structures
tsOTA_QueryImageRequest#
The following structure contains payload data for a Query Next Image Request issued by a client to poll the server for an upgrade image or to respond to an Image Notify message from the server:
typedef struct
{
uint32 u32CurrentFileVersion;
uint16 u16HardwareVersion;
uint16 u16ImageType;
uint16 u16ManufacturerCode;
uint8 u8FieldControl;
}tsOTA_QueryImageRequest;
where:
u32CurrentFileVersionis the file version of the application image that is currently running on the client that sent the requestu16HardwareVersionis the hardware version of the client device (this information is optional - seeu8FieldControlbelow)u16ImageTypeis a value in the range 0x0000-0xFFBF which identifies the type of image currently running on the clientu16ManufacturerCodeis the ZigBee-assigned number identifying the manufacturer of the client deviceu8FieldControlis a bitmap indicating whether certain optional information about the client is included in this Query Next Image Request message. Currently, this optional information consists only of the hardware version (contained inu16HardwareVersionabove) - bit 0 is set to ‘1’ if the hardware version is included or to ‘0’ otherwise (all other bits are reserved)
Parent topic:Structures
tsOTA_QueryImageResponse#
The following structure contains payload data for a Query Next Image Response issued by the server (as the result of a Query Next Image Request from a client):
typedef struct
{
uint32 u32ImageSize;
uint32 u32FileVersion;
uint16 u16ManufacturerCode;
uint16 u16ImageType;
uint8 u8Status;
}tsOTA_QueryImageResponse;
where:
u32ImageSizeis the total size of the available image, in bytesu32FileVersionis the file version of the available imageu16ManufacturerCodeis the manufacturer code that was received from the client in the Query Next Image Request messageu16ImageTypeis the image type that was received from the client in the Query Next Image Request messageu8Statusindicates whether a suitable image is available for download:OTA_STATUS_SUCCESS: A suitable image is available
OTA_STATUS_NO_IMAGE_AVAILABLE: No suitable image is available
The other elements of the structure are only included in the case of success.
Parent topic:Structures
tsOTA_BlockRequest#
The following structure contains payload data for an Image Block Request issued by a client to request an image data block from the server:
typedef struct
{
uint64 u64RequestNodeAddress;
uint32 u32FileOffset;
uint32 u32FileVersion;
uint16 u16ImageType;
uint16 u16ManufactureCode;
uint16 u16BlockRequestDelay;
uint8 u8MaxDataSize;
uint8 u8FieldControl;
}tsOTA_BlockRequest;
where:
u64RequestNodeAddressis the IEEE/MAC address of the client device from which the request originates (this information is optional - seeu8FieldControlbelow)u32FileOffsetspecifies the offset from the beginning of the upgrade image, in bytes, of the requested data block (this value is therefore determined by the amount of image data previously received)u32FileVersionis the file version of the upgrade image for which a data block is being requestedu16ImageTypeis a value in the range 0x0000-0xFFBF which identifies the type of image for which a data block is being requestedu16ManufactureCodeis the ZigBee-assigned number identifying the manufacturer of the client device from which the request originatesu16BlockRequestDelayis used in ‘rate limiting’ to specify the value of the ‘block request delay’ attribute for the client - this is minimum time, in milliseconds, that the client must wait between consecutive block requests (the client will update the local attribute with this value). If the server does not support rate limiting or does not need to limit the download rate to the client, this field will be set to 0u8MaxDataSizespecifies the maximum size, in bytes, of the data block that the client can receive in one transfer (the server must therefore not send a data block that is larger than indicated by this value)u8FieldControlis a bitmap indicating whether certain optional information about the client is included in this Image Block Request message. Currently, this optional information consists only of the IEEE/MAC address of the client (contained in64RequestNodeAddressabove) - bit 0 is set to ‘1’ if this address is included or to ‘0’ otherwise (all other bits are reserved)
Parent topic:Structures
tsOTA_ImagePageRequest#
The following structure contains payload data for an Image Page Request issued by a client to request a page of image data (multiple blocks) from the server:
typedef struct
{
uint64 u64RequestNodeAddress;
uint32 u32FileOffset;
uint32 u32FileVersion;
uint16 u16PageSize;
uint16 u16ResponseSpacing;
uint16 u16ImageType;
uint16 u16ManufactureCode;
uint8 u8MaxDataSize;
uint8 u8FieldControl;
}tsOTA_ImagePageRequest;
where:
u64RequestNodeAddressis the IEEE/MAC address of the client device from which the request originates (this information is optional - seeu8FieldControlbelow)u32FileOffsetspecifies the offset from the beginning of the upgrade image, in bytes, of the first data block of the requested page (this value is therefore determined by the amount of image data previously received)u32FileVersionis the file version of the upgrade image for which data is being requestedu16PageSizeis the total number of data bytes (in the page) to be returned by the server before the next Image Page Request can be issued (this must be larger than the value ofu8MaxDataSizebelow)u16ResponseSpacingspecifies the time-interval, in milliseconds, that the server should introduce between consecutive transmissions of Image Block Responses (which is sent in response to the Image Page Request)u16ImageTypeis a value in the range 0x0000-0xFFBF which identifies the type of image for which data is being requestedu16ManufactureCodeis the ZigBee-assigned number identifying the manufacturer of the client device from which the request originatesu8MaxDataSizespecifies the maximum size, in bytes, of the data block that the client can receive in one transfer (the server must therefore not send a data block in an Image Block Response that is larger than indicated by this value)u8FieldControlis a bitmap indicating whether certain optional information about the client is included in this Image Page Request message. Currently, this optional information consists only of the IEEE/MAC address of the client (contained in64RequestNodeAddressabove) - bit 0 is set to ‘1’ if this address is included or to ‘0’ otherwise (all other bits are reserved)
Parent topic:Structures
tsOTA_ImageBlockResponsePayload#
The following structure contains payload data for an Image Block Response issued by the server (as the result of an Image Block Request from a client):
typedef struct
{
uint8 u8Status;
union
{
tsOTA_WaitForData sWaitForData;
tsOTA_SuccessBlockResponsePayload sBlockPayloadSuccess;
}uMessage;
}tsOTA_ImageBlockResponsePayload;
where:
u8Statusindicates whether a data block is included in the response:OTA_STATUS_SUCCESS: A data block is included
OTA_STATUS_WAIT_FOR_DATA: No data block is included - client should re-request a data block after a waiting time
The element used from the union depends on the status reported above:
sWaitForDatais a structure containing information used to instruct the requesting client to wait for a time before requesting the data block again or requesting the next data block (see Section 49.11.15) - this information is only provided in the case of the status OTA_STATUS_WAIT_FOR_DATAsBlockPayloadSuccessis a structure containing a requested data block and associated information (see Section 49.11.13) - this data is only provided in the case of the status OTA_STATUS_SUCCESS
Parent topic:Structures
tsOTA_UpgradeEndRequestPayload#
The following structure contains payload data for an Upgrade End Request issued by a client to terminate/close an image download from the server:
typedef struct
{
uint32 u32FileVersion;
uint16 u16ImageType;
uint16 u16ManufacturerCode;
uint8 u8Status;
}tsOTA_UpgradeEndRequestPayload;
where:
u32FileVersionis the file version of the upgrade image which has been downloadedu16ImageTypeis the type of the upgrade image which has been downloadedu16ManufacturerCodeis the ZigBee-assigned number identifying the manufacturer of the client device from which the request originatesu8Statusis the reported status of the image download, one of:OTA_STATUS_SUCCESS (successfully downloaded and verified)
OTA_STATUS_INVALID_IMAGE (downloaded but failed verification)
OTA_REQUIRE_MORE_IMAGE (other images needed)
OTA_STATUS_ABORT (download in progress is to be aborted)
Parent topic:Structures
tsOTA_UpgradeEndResponsePayload#
The following structure contains payload data for an Upgrade End Response issued by the server (as the result of an Upgrade End Request from a client):
typedef struct
{
uint32 u32UpgradeTime;
uint32 u32CurrentTime;
uint32 u32FileVersion;
uint16 u16ImageType;
uint16 u16ManufacturerCode;
}tsOTA_UpgradeEndResponsePayload;
where:
u32UpgradeTimeis the UTC time, in seconds, at which the client should upgrade the running image with the downloaded image. If the server does not support UTC time (indicated by a zero value foru32CurrentTime), the client should interpret this value as a time delay before performing the image upgradeu32CurrentTimeis the current UTC time, in seconds, on the server. If UTC time is not supported by the server, this value should be set to zero. If this value is set to 0xFFFFFFFF, this indicates that the client should wait for an upgrade command from the server before performing the image upgrade
Note: If the client does not support UTC time but both of the above time values are non-zero, the client will take the difference between the two times as a time delay before performing the image upgrade.
u32FileVersionis the file version of the downloaded application image (a wild card value of 0xFFFFFFFF can be used when the same response is sent to client devices from different manufacturers)u16ImageTypeis the type of the downloaded application image (a wild card value of 0xFFFF can be used when the same response is sent to client devices from different manufacturers)u16ManufacturerCodeis the manufacturer code that was received from the client in the Upgrade End Request message (a wild card value of 0xFFFF can be used when the same response is sent to client devices from different manufacturers)
Parent topic:Structures
tsOTA_SuccessBlockResponsePayload#
The following structure contains payload data for an Image Block Response which reports ‘success’ and therefore contains a block of image data (see Section 49.11.10):
typedef struct
{
uint8* pu8Data;
uint32 u32FileOffset;
uint32 u32FileVersion;
uint16 u16ImageType;
uint16 u16ManufacturerCode;
uint8 u8DataSize;
}tsOTA_SuccessBlockResponsePayload;
where:
pu8Datais a pointer to the start of the data block being transferredu32FileOffsetis the offset, in bytes, of the start of the data block from the start of the image (normally, the same offset as specified in the Image Block Request)u32FileVersionis the file version of the upgrade image to which the included data block belongsu16ImageTypeis the type of the upgrade image to which the included data block belongsu16ManufacturerCodeis the manufacturer code that was received from the client in the Image Block Requestu8DataSizeis the length, in bytes, of the included data block (this must be less than or equal to the maximum data block length for the client, specified in the Image Block Request)
Parent topic:Structures
tsOTA_BlockResponseEvent#
The following structure contains payload data for an Image Block Response containing data other than upgrade image data.
typedef struct
{
uint8 u8Status;
uint8 *pu8Data;
uint8 u8DataSize;
}tsOTA_BlockResponseEvent;
where:
u8Statusindicates whether a suitable upgrade image is available:OTA_STATUS_SUCCESS: A suitable image is available
OTA_STATUS_NO_IMAGE_AVAILABLE: No suitable image is available
pu8Datais a pointer to the start of the data block being transferredu8DataSizeis the length, in bytes, of the included data block (this must be less than or equal to the maximum data block length for the client, specified in the Image Block Request)
Parent topic:Structures
tsOTA_WaitForData#
The following structure contains time information for an Image Block Response. It can be used by a response which reports ‘failure’, to instruct the client to re-request the data block after a certain waiting time (see Section 49.11.10). It can also be used in ‘rate limiting’ to specify a new value for the ‘block request delay’ attribute on the client.
typedef struct
{
uint32 u32CurrentTime;
uint32 u32RequestTime;
uint16 u16BlockRequestDelayMs;
}tsOTA_WaitForData;
where:
u32CurrentTimeis the current UTC time, in seconds, on the server. If UTC time is not supported by the server, this value should be set to zerou32RequestTimeis the UTC time, in seconds, at which the client should re-issue an Image Block Request. If the server does not support UTC time (indicated by a zero value foru32CurrentTime), the client should interpret this value as a time delay before re-issuing an Image Block Request
Note: If the client does not support UTC time but both of the above values are non-zero, the client will take the difference between the two times as a time delay before re-issuing an Image Block Request.
u16BlockRequestDelayMsis used in ‘rate limiting’ to specify the value of the ‘block request delay’ attribute for the client - this is minimum time, in milliseconds, that the client must wait between consecutive block requests (the client will update the local attribute with this value). If the server does not support rate limiting or does not need to limit the download rate to the client, this field must be set to 0
Parent topic:Structures
tsOTA_WaitForDataParams#
The following structure is used in the tsOTA_CallBackMessage structure (see Section 49.11.21) on an OTA Upgrade server. It contains the data needed to notify a client that rate limiting is required or the client must wait to receive an upgrade image.
typedef struct
{
bool_t bInitialized;
uint16 u16ClientAddress;
tsOTA_WaitForData sWaitForDataPyld;
}tsOTA_WaitForDataParams;
where:
bInitializedis a boolean flag indicating the server’s request to the client:TRUE - Implement rate limiting or wait to receive upgrade image
FALSE - Otherwise
u16ClientAddresscontains the 16-bit network address of the clientsWaitForDataPyldis a structure containing the payload for an Image Block Response with status OTA_STATUS_WAIT_FOR_DATA (see Section49.11.15)
Parent topic:Structures
tsOTA_PageReqServerParams#
The following structure is used in the tsOTA_CallBackMessage structure (see Section 49.11.21) on an OTA Upgrade server. It contains the data from an Image Page Request received from a client.
typedef struct
{
uint8 u8TransactionNumber;
bool_t bPageReqRespSpacing;
uint16 u16DataSent;
tsOTA_ImagePageRequest sPageReq;
tsZCL_ReceiveEventAddress sReceiveEventAddress;
}tsOTA_PageReqServerParams;
where:
u8TransactionNumberis the Transaction Sequence Number (TSN) which is used in the Image Page RequestbPageReqRespSpacingis a boolean used to request a spacing between consecutive Image Block Responses:TRUE - Implement spacing
FALSE - Otherwise
u16DataSentindicates the number of data bytes contained in the Image Page RequestsPageReqis a structure containing the payload data from the Image Page Request (see Section 49.11.9)sReceiveEventAddresscontains the address of the OTA Upgrade client that made the page request
Parent topic:Structures
tsOTA_PersistedData#
The following structure contains the persisted data that is stored in Flash memory using the NVM module:
typedef struct
{
tsCLD_AS_Ota sAttributes;
uint32 u32FunctionPointer;
uint32 u32RequestBlockRequestTime;
uint32 u32CurrentFlashOffset;
uint32 u32TagDataWritten;
uint32 u32Step;
uint16 u16ServerShortAddress;
#ifdef OTA_CLD_ATTR_REQUEST_DELAY
bool_t bWaitForBlockReq;
#endif
uint8 u8ActiveTag[OTA_TAG_HEADER_SIZE];
uint8 u8PassiveTag[OTA_TAG_HEADER_SIZE];
uint8 au8Header[OTA_MAX_HEADER_SIZE];
uint8 u8Retry;
uint8 u8RequestTransSeqNo;
uint8 u8DstEndpoint;
bool_t bIsCoProcessorImage;
bool_t bIsSpecificFile;
bool_t bIsNullImage;
uint8 u8CoProcessorOTAHeaderIndex;
uint32 u32CoProcessorImageSize;
uint32 u32SpecificFileSize;
#ifdef OTA_PAGE_REQUEST_SUPPORT
tsOTA_PageReqParams sPageReqParams;
#endif
#if (OTA_MAX_CO_PROCESSOR_IMAGES != 0)
uint8 u8NumOfDownloadableImages;
#endif
#ifdef OTA_INTERNAL_STORAGE
uint8 u8Buf[4];
#endif
}tsOTA_PersistedData;
The fields are for internal use and no knowledge of them is required.
Parent topic:Structures
tsOTA_QuerySpecificFileRequestPayload#
The following structure contains the payload for a Query Specific File Request which is issued by an OTA Upgrade client to request a device-specific file from the server.
typedef struct
{
uint64 u64RequestNodeAddress;
uint16 u16ManufacturerCode;
uint16 u16ImageType;
uint32 u32FileVersion;
uint16 u16CurrentZibgeeStackVersion;
}tsOTA_QuerySpecificFileRequestPayload;
where:
u64RequestNodeAddressis the IEEE/MAC address of the node requesting the device-specific file from the serveru16ManufactuerCodeis the ZigBee-assigned manufacturer code of the requesting node (0xFFFF is used to indicate any manufacturer)u16ImageTypeindicates the requested file type - one of the reserved values that are assigned to the device-specific file types (the value should be in the range 0xFFC0 to 0xFFFE, but only 0xFFC0 to 0xFFC2 are currently in use)32FileVersioncontains the release and build numbers of the application and stack that correspond to the device-specific file - for details of the format, refer to the ZigBee Over-the-Air Upgrading Cluster Specification (095264)u16CurrentZ``ig``beeStackVersioncontains the version of ZigBee stack that is currently running on the client
Parent topic:Structures
tsOTA_QuerySpecificFileResponsePayload#
The following structure contains the payload for a Query Specific File Response which is issued by an OTA Upgrade server in response to a request for a device-specific file.
typedef struct
{
uint32 u32FileVersion;
uint32 u32ImageSize;
uint16 u16ImageType;
uint16 u16ManufacturerCode;
uint8 u8Status;
}tsOTA_QuerySpecificFileResponsePayload;
where:
32FileVersioncontains the release and build numbers of the application and stack that correspond to the device-specific file - this field will take the same value as the equivalent field in the corresponding Query Specific File Request (see Section 49.11.19)u32ImageSizeis the size of the requested file, in bytesu16ImageTypeindicates the requested file type - this field will take the same value as the equivalent field in the corresponding Query Specific File Request (see Section 49.11.19)u16ManufactuerCodeis the ZigBee-assigned manufacturer code of the requesting node - this field will take the same value as the equivalent field in the corresponding Query Specific File Request (see Section 49.11.19)u8Statusindicates whether a suitable file is available for download:OTA_STATUS_SUCCESS: A suitable file is available
OTA_STATUS_NO_IMAGE_AVAILABLE: No suitable file is available
The other elements of the structure are only included in the case of success.
Parent topic:Structures
tsOTA_CallBackMessage#
For an OTA event, the eEventType field of the tsZCL_CallBackEvent structure is set to E_ZCL_CBET_CLUSTER_CUSTOM. This event structure also contains an element sClusterCustomMessage, which is itself a structure containing a field pvCustomData. This field is a pointer to the following tsOTA_CallBackMessage structure:
typedef struct
{
teOTA_UpgradeClusterEvents eEventId;
#ifdef OTA_CLIENT
tsOTA_PersistedData sPersistedData;
uint8 au8ReadOTAData[OTA_MAX_BLOCK_SIZE];
uint8 u8NextFreeImageLocation;
uint8 u8CurrentActiveImageLocation;
#endif
#ifdef OTA_SERVER
tsCLD_PR_Ota aServerPrams[OTA_MAX_IMAGES_PER_ENDPOINT+OTA_MAX_CO_PROCESSOR_IMAGES];
tsOTA_AuthorisationStruct sAuthStruct;
uint8 u8ServerImageStartSector;
bool bIsOTAHeaderCopied;
uint8 au8ServerOTAHeader[OTA_MAX_HEADER_SIZE+OTA_TAG_HEADER_SIZE];
tsOTA_WaitForDataParams sWaitForDataParams;
#ifdef OTA_PAGE_REQUEST_SUPPORT
tsOTA_PageReqServerParams sPageReqServerParams;
#endif
#endif
uint8 u8ImageStartSector[OTA_MAX_IMAGES_PER_ENDPOINT];
uint8 au8CAPublicKey[22];
uint8 u8MaxNumberOfSectors;
union
{
tsOTA_ImageNotifyCommand sImageNotifyPayload;
tsOTA_QueryImageRequest sQueryImagePayload;
tsOTA_QueryImageResponse sQueryImageResponsePayload;
tsOTA_BlockRequest sBlockRequestPayload;
tsOTA_ImagePageRequest sImagePageRequestPayload;
tsOTA_ImageBlockResponsePayload sImageBlockResponsePayload;
tsOTA_UpgradeEndRequestPayload sUpgradeEndRequestPayload;
tsOTA_UpgradeEndResponsePayload sUpgradeResponsePayload;
tsOTA_QuerySpecificFileRequestPayload sQuerySpFileRequestPayload;
tsOTA_QuerySpecificFileResponsePayload
sQuerySpFileResponsePayload;
teZCL_Status eQueryNextImgRspErrStatus;
tsOTA_SignerMacVerify sSignerMacVerify;
tsOTA_ImageVersionVerify sImageVersionVerify;
tsOTA_UpgradeDowngradeVerify sUpgradeDowngradeVerify;
}uMessage;
}tsOTA_CallBackMessage;
where:
eEventIdis the OTA event type (enumerations are detailed in Section49.12.2)sPersistedDatais the structure (see Section 49.11.18) which contains the persisted data that is stored in Flash memory using the NVM module on the clientau8ReadOTADatais an array containing the payload data from an Image Block Responseu8NextFreeImageLocationidentifies the next free image location where a new upgrade image can be storedu8CurrentActiveImageLocationidentifies the location of the currently active image on the clientaServerPramsis an array containing the server data for each image which can be updated by applicationsAuthStructis a structure which stores the authorisation state and list of client devices that are authorised for OTA upgradeu8ServerImageStartSectoridentifies the server self-image start-sectorbIsOTAHeaderCopiedspecifies whether the new OTA header is copied (TRUE) or not (FALSE)au8ServerOTAHeaderspecifies the current server OTA headersWaitForDataParamsis a structure containing time information that may need to be modified by the server for inclusion in an Image Block Response (for more information, refer to Section 49.11.15)sPageReqServerParamsis a structure containing page request information that may need to be modified by the serveru8ImageStartSectoris used to store the image start-sector for each image which is stored or will be stored in the devices internal Flash memory - note that this variable assumes a 32-Kbyte sector size and so, for example, if64-Kbyte sectors are used, its value will be twice the actual start-sector value
au8CAPublicKeyspecifies the CA public keyu8MaxNumberOfSectorsspecifies the maximum number of sectors to be used per imageuMessageis a union containing the command payload in one of the following forms (depending on the command specified byeEventId):sImageNotifyPayloadis a structure containing the payload of an Image Notify commandsQueryImagePayloadis a structure containing the payload of a Query Next Image RequestsQueryImageResponsePayloadis a structure containing the payload of a Query Next Image ResponsesBlockRequestPayloadis a structure containing the payload of an Image Block RequestsImagePageRequestPayloadis a structure containing the payload of an Image Page RequestsImageBlockResponsePayloadis a structure containing the payload of an Image Block ResponsesUpgradeEndRequestPayloadis a structure containing the payload of an Upgrade End RequestsUpgradeResponsePayloadis a structure containing the payload of an Upgrade End ResponsesQuerySpFileRequestPayloadis a structure containing the payload of a Query Specific File RequestsQuerySpFileResponsePayloadis a structure containing the payload of a Query Specific File ResponseeQueryNextImgRspErrStatusis the status returned from the query image response command handler and can be passed up to the application when there is an error via the callback event E_CLD_OTA_COMMAND_QUERY_NEXT_IMAGE_RESPONSE_ERROR. The returned status value will be either E_ZCL_ERR_INVALID_IMAGE_SIZE or E_ZCL_ERR_INVALID_IMAGE_VERSION
sSignerMacVerifyis a structure containing the signer’s IEEE/MAC address from a new upgrade image and a status field (which is set by the application after verifying the signer’s address)sImageVersionVerifyis a structure containing the image version received in the query next image response and status field (which is set by the application after verifying the image version)sUpgradeDowngradeVerifyis a structure containing the image version received in the upgrade end response and a status field (which is set by the application after verifying the image version)
Parent topic:Structures
tsCLD_PR_Ota#
The following structure contains server parameter data that can be pre-set using the function eOTA_SetServerParams() and obtained using eOTA_GetServerData():
typedef struct
{
uint8* pu8Data;
uint32 u32CurrentTime;
uint32 u32RequestOrUpgradeTime;
uint8 u8QueryJitter;
uint8 u8DataSize;
} tsCLD_PR_Ota;
where:
pu8Datais a pointer to the start of a block of datau32CurrentTimeis the current UTC time, in seconds, on the server. If UTC time is not supported by the server, this value should be set to zerou32RequestOrUpgradeTimeis used by the server as the ‘request time’ and the ‘upgrade time’ when sending responses to clients:As a ‘request time’, the value may be included in an Image Block Response (see Section 49.11.10 and Section 49.11.15)
As an ‘upgrade time’, the value will be included in an Upgrade End Response (see Section 49.11.12)
u8QueryJitteris a value between 1 and 100 (inclusive) which is used by a receiving client to decide whether to reply to an Image Notify message - for information on ‘Query Jitter’, refer to Section 49.7u8DataSizeis the length, in bytes, of the data block pointed to bypu8Data
Parent topic:Structures
tsCLD_AS_Ota#
This structure contains attribute values which are stored as part of the persisted data in Flash memory:
typedef struct
{
uint64 u64UgradeServerID;
uint32 u32FileOffset;
uint32 u32CurrentFileVersion;
uint16 u16CurrentStackVersion;
uint32 u32DownloadedFileVersion;
uint16 u16DownloadedStackVersion;
uint8 u8ImageUpgradeStatus;
uint16 u16ManfId;
uint16 u16ImageType;
uint16 u16MinBlockRequestDelay;
} tsCLD_AS_Ota;
where the structure elements are OTA Upgrade cluster attribute values, as described in [Section 49.3](ota_upgrade_cluster_structure_and_attributes.md#id_accc84e1-e4af-4078-b61f-af69b4b4314c).
Parent topic:Structures
tsOTA_ImageVersionVerify#
The following structure contains the data for an event of the type E_CLD_OTA_INTERNAL_COMMAND_VERIFY_IMAGE_VERSION.
typedef struct
{
uint32 u32NotifiedImageVersion;
uint32 u32CurrentImageVersion;
teZCL_Status eImageVersionVerifyStatus;
}tsOTA_ImageVersionVerify;
where:
u32NotifiedImageVersionis the version received in the query next image responseu32CurrentImageVersionis the version of the running imageeImageVersionVerifyStatusis a status field which should be updated to E_ZCL_SUCCESS or E_ZCL_FAIL by the application after checking the received image version, to indicate whether the upgrade image has a valid image version
Parent topic:Structures
tsOTA_UpgradeDowngradeVerify#
The following structure contains the data for an event of the type E_CLD_OTA_INTERNAL_COMMAND_SWITCH_TO_UPGRADE_DOWNGRADE.
typedef struct
{
uint32 u32DownloadImageVersion;
uint32 u32CurrentImageVersion;
teZCL_Status eUpgradeDowngradeStatus;
}tsOTA_UpgradeDowngradeVerify;
where:
u32DownloadImageVersionis the version received in upgrade end responseu32CurrentImageVersionis the version of running imageeImageVersionVerifyStatusis a status field which should be updated to E_ZCL_SUCCESS or E_ZCL_FAIL by the application after checking the received image version, to indicate whether the upgrade image has a valid image version
Parent topic:Structures
Parent topic:OTA Upgrade cluster