MCUXpresso SDK Documentation

tsOTA_ImageHeader

tsOTA_ImageHeader#

The following structure contains information for the OTA header:

typedef struct
{
            uint32 u32FileIdentifier;
    uint16 u16HeaderVersion;
    uint16 u16HeaderLength;
    uint16 u16HeaderControlField;
    uint16 u16ManufacturerCode;
    uint16 u16ImageType;
    uint32 u32FileVersion;
    uint16 u16StackVersion;
    uint8  stHeaderString[OTA_HEADER_STRING_SIZE];
            uint32 u32TotalImage;
    uint8  u8SecurityCredVersion;
    uint64 u64UpgradeFileDest;
    uint16 u16MinimumHwVersion;
    uint16 u16MaxHwVersion;
}tsOTA_ImageHeader;

where:

  • u32FileIdentifier is a 4-byte value equal to 0x0BEEF11E which indicates that the file contains an OTA upgrade image

  • u16HeaderVersion is the version of the OTA header expressed as a 2-byte value in which the most significant byte contains the major version number and the least significant byte contains the minor version number

  • u16HeaderLength is the full length of the OTA header, in bytes

  • u16HeaderControlField is a bitmap indicating certain information about the file, as detailed in table below.

Bit

Information

0

Security credential version (in OTA header):

1: Field present in header

0: Field not present in header

| |1|Device-specific file (also see u64UpgradeFileDest):

1: File is device-specific

0: File is not device-specific

| |2|Maximum and minimum hardware version (in OTA header):

1: Field present in header

0: Field not present in header

| |3-15|Reserved|

  • u16ManufacturerCode is the ZigBee-assigned manufacturer code (0xFFFF is a wildcard value, representing any manufacturer)

  • u16ImageType is a unique value representing the image type, where this value is normally manufacturer-specific but certain values have been reserved for specific file types, as indicated below (the wildcard value of 0xFFFF represents any file type):

Value

File Type

0x0000 – 0xFFBF

Manufacturer-specific

0xFFC0

Security credential

0xFFC1

Configuration

0xFFC2

Log

0xFFC3 – 0xFFFE

Reserved

0xFFFF

Wildcard

  • u32FileVersion contains the release and build numbers of the application and stack used to produce the application image - for details of the file version format, refer to         the ZigBee Over-the-Air Upgrading Cluster Specification (095264)

  • u16StackVersion contains ZigBee stack version that is used by the application (this is 0x0002 for ZigBee PRO)

  • stHeaderString[] is a manufacturer-specific string that can be used to store any useful human-readable information

  • u32TotalImage is the total size, in bytes, of the image that will be transferred over-the air (including the OTA header and any optional data)

  • u8SecurityCredVersion indicates the security credential version type that is required by the client in order to install the image - the possibilities are SE1.0 (0x0), SE1.1 (0x1) and SE2.0 (0x2)

  • u64UpgradeFileDest contains the IEEE/MAC address of the destination device for the file, in the case when the file is device-specific (as indicated by bit 1 of u16HeaderControlField)

  • u16MinimumHwVersion indicates the earliest hardware platform on which the image should be used, expressed as a 2-byte value in which the most significant byte contains the hardware version number and the least significant byte contains the revision number

  • u16MaxHwVersion indicates the latest hardware platform on which the image should be used, expressed as a 2-byte value in which the most significant byte contains the hardware version number and the least significant byte contains the revision number

Parent topic:Structures