tsOTA_QuerySpecificFileRequestPayload#
The following structure contains the payload for a Query Specific File Request which is issued by an OTA Upgrade client to request a device-specific file from the server.
typedef struct
{
uint64 u64RequestNodeAddress;
uint16 u16ManufacturerCode;
uint16 u16ImageType;
uint32 u32FileVersion;
uint16 u16CurrentZibgeeStackVersion;
}tsOTA_QuerySpecificFileRequestPayload;
where:
u64RequestNodeAddressis the IEEE/MAC address of the node requesting the device-specific file from the serveru16ManufactuerCodeis the ZigBee-assigned manufacturer code of the requesting node (0xFFFF is used to indicate any manufacturer)u16ImageTypeindicates the requested file type - one of the reserved values that are assigned to the device-specific file types (the value should be in the range 0xFFC0 to 0xFFFE, but only 0xFFC0 to 0xFFC2 are currently in use)32FileVersioncontains the release and build numbers of the application and stack that correspond to the device-specific file - for details of the format, refer to the ZigBee Over-the-Air Upgrading Cluster Specification (095264)u16CurrentZ``ig``beeStackVersioncontains the version of ZigBee stack that is currently running on the client
Parent topic:Structures