eCLD_OnOffCommandOffWithEffectSend#
teZCL_Status eCLD_OnOffCommandOffWithEffectSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_OnOff_OffWithEffectRequestPayload *psPayload);
Description#
This function sends a custom ‘Off With Effect’ command instructing the target lighting device to switch off one or more lights with the specified effect, which can be one of:
fade (in two phases or no fade)
rise and fall
Each of these effects is available in variants. The required effect and variant are specified in the command payload. For the payload details, refer to “Off With Effect Request Payload “.
The device receiving this message generates a callback event on the endpoint on which the On/Off cluster was registered.
Following a call to this function, the light settings on the target device are saved to a global scene, after which the attribute bGlobalSceneControl is set to FALSE - for more details, refer to Section 14.6.
If used, the ‘Off With Effect’ command must be enabled in the compile-time options on both the client and server, as described in Section 14.10.
Parameters#
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types
eZCL_AMBOUND and eZCL_AMGROUP.psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.
psPayload: Pointer to a structure containing the payload for this message (see Section 14.8.2).
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions