eCLD_ScenesCommandRemoveAllScenesRequestSend#
teZCL_Status eCLD_ScenesCommandRemoveAllScenesRequestSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_ScenesRemoveAllScenesRequestPayload
Description#
This function sends a Remove All Scenes command to request that the target device deletes all entries corresponding to the specified group ID/address in its Scene table. The relevant group ID is specified in the payload of the message. Note that specifying a group ID of 0x0000 removes all scenes not associated with a group.
The device receiving this message generates a callback event on the endpoint on which the Scenes cluster was registered. The device then deletes the scenes in the Scene table. If the request is sent to a single device (rather than to a group address), it then generates an appropriate Remove All Scenes response indicating success, or failure (see Section 13.7.3).
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters#
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.
psPayload: Pointer to a structure containing the payload for this message (see Section 13.7.2).
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions