tsZCL_AttributeDefinition#
This structure defines an attribute used in a cluster:
struct tsZCL_AttributeDefinition
{
uint16 u16AttributeEnum;
uint8 u8AttributeFlags;
teZCL_ZCLAttributeType eAttributeDataType;
uint16 u16OffsetFromStructBase;
uint16 u16AttributeArrayLength;
};
Where:
u16AttributeEnumis the Attribute ID.u8AttributeFlagsis a 5-bit bitmap indicating the accessibility of the attribute (for details of the access types, refer to Section 2.3.1) - a bit is set to ‘1’ if the corresponding access type is supported, as follows:
Bit |
Access Type |
|---|---|
0 |
Read |
1 |
Write |
2 |
Reportable |
3 |
Scene |
4 |
Global |
5-7 |
Reserved |
eAttributeDataTypeis the data type of the attribute - see Section 7.1.3.u16O``ffsetFromStructBaseis the offset of the attribute’s location from the start of the cluster.u16AttributeArrayLengthis the number of consecutive attributes of the same type.
Parent topic:General Structures