MCUXpresso SDK Documentation

Install CMSIS device pack

Install CMSIS device pack#

After the MDK tools are installed, Cortex Microcontroller Software Interface Standard (CMSIS) device packs must be installed to fully support the device from a debug perspective. These packs include things such as memory map information, register definitions and flash programming algorithms. Follow these steps to install the MIMXRT106x CMSIS pack.

  1. Download the MIMXRT1061 and MIMXRT1062 packs.

  2. After downloading the DFP, double click to install it.

Parent topic:Run a demo using Keil MDK/μVision