freertos_lpspi_b2b_master#
Overview#
The freertos_lpspi_b2b_master example shows how to use LPSPI driver in FreeRTOS. In this example are required two boards, one board is used as LPSPI master on which is runnuing freertos_lpspi_b2b_master and another board is used as LPSPI slave on which is running freertos_lpspi_b2b_slave example.
Connection of boards is in section Board settings.
It is required to run first the slave demo.
Running the demo#
When the example runs successfully, you can see the similar information from the terminal as below. If runs on one single board:
FreeRTOS LPSPI master example starts.
This example uses two boards to connect with one as master and anohter as slave.
Master and slave are both use interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
LPSPI_master -- LPSPI_slave
CLK -- CLK
PCS -- PCS
SOUT -- SIN
SIN -- SOUT
LPSPI master transfer completed successfully.
LPSPI transfer all data matched !