Setting up ZigBee security#
This section describes how to set up ZigBee security in your application code. Note that if security is enabled in a ZigBee network then network-level security is always used, while application-level security is optional.
Security is enabled on a node via the device parameter Security Enabledin the ZPS Configuration Editor. Enabling security also enables many-to-one routing toward the Trust Centre, which becomes a network concentrator (see Section 3.5.3).
A Trust Centre must be nominated (see Section 2.8) using the ZPS Configuration Editor. The Coordinator is normally chosen as the Trust Centre. The maximum number of nodes that will require the services of the Trust Centre must be set on the nominated node using the network parameter Route Record Table Sizein the ZPS Configuration Editor (the default number is 4).
Security can be set up in the application code using the function zps_vAplSecSetInitialSecurityState(), which must be called before zps_eAplAfInit() and zps_eAplZdoStartStack() - see Section 6.1.
Note: As an alternative to using the function zps_vAplSecSetInitialSecurityState() in the application code, ZigBee security can be set up in the ZPS Configuration Editor (see Section 6.8.3.1).
Once zps_vAplSecSetInitialSecurityState() has been called and the stack has been started, the stack will automatically manage the subsequent network-level security set-up and implementation.
Network-level security set-up and application-level security set-up are further described in Section 6.8.3.1 and Section 6.8.3.2 respectively.
Note: Certain functionality on the Trust Centre can be disabled using the zps_vSetTCLockDownOverride() function. For more information, refer to the function description.
Network-level security set-up#
The function zps_vAplSecSetInitialSecurityState(), described above, initiates the set-up process for network-level security and requires the type of initial security key to be specified as one of:
Pre-configured global link key
Pre-configured unique link key
These keys are described in Section 5.8.2. They are used to encrypt the network key when it is transported to a joining node.
The Trust Centre and other nodes must be pre-programmed with the relevant pre- configured link key(s). This key can be specified in the application code for the node and referenced by zps_vAplSecSetInitialSecurityState() or can be set through the Key Descriptor parameter Keyin the ZPS Configuration Editor on both the Trust Centre and other node(s). In the case of a unique link key, the IEEE/MAC address of the node must also be pre-programmed into the Trust Centre along with the link key. For the Key Descriptor parameters, refer to Section 11.7.9.
Note: Pre-configured link keys entered via the ZPS Configuration Editor are held in a Key Descriptor Table on the Trust Centre, with one entry for each node/key. The key for a node with a given IEEE/MAC address can be obtained (locally) from this table using the function zps_psGetActiveKey().
The Trust Centre generates a random network key to be used in network-level communications between all nodes. When a new node joins the network, the Trust Centre transports this network key, encrypted using the appropriate pre-configured link key, to the newly joined node.
Note:
The application on the Trust Centre can take control (from the stack) of whether a node is allowed to join the network (possibly using its pre-configured link key) through a user-defined callback function. If required, this callback function must be registered using the function zps_vTCSetCallback(). For more details, refer to the function description.
When a device joins a ZigBee network and requires authentication which involves transporting a network key to it, the parent opens an authentication interval during which the joining device must announce itself to the network. This interval begins from the transmission of a rejoin response (if the device joins through a NWK layer rejoin) or an association response (if it joins through an IEEE 802.15.4 association). If the device fails to announce itself during this interval, the parent removes the Neighbor table entry for the joining device to ensure that the child capacity of the parent is maintained. This authentication interval must be set on all potential parent nodes via the network parameter APS Security Timeout Period (see Section 11.7), which is 1 second by default but 6 seconds is a more reasonable setting.
Parent topic:Setting up ZigBee security
Application-level security set-up#
Once network-level security has been set up (as described in Section 6.8.3.1), application-level security can be set up, if required. In application-level security, the communications between two nodes are encrypted/decrypted using a link key which may be global or unique:
Global link key: This is shared between all nodes on the network and is pre- configured in all the nodes. Frame counters are not checked for freshness when using a global link key.
Unique link key: This is exclusive to a pair of nodes that need to communicate privately. It may be a pre-configured unique link key, Trust Centre Link Key (TCLK) or application link key. Frame counters are checked for freshness to prevent rogue nodes replaying stale messages. This provides the most secure method of application security.
The different types of link key are described in Section 6.8.2 and summarized in Table 4.
In order to set up application-level security with a unique link key between two nodes, the function zps_eAplZdoRequestKeyReq() must be called on one of the nodes to request a link key from the Trust Centre. There are two possibilities:
To request a Trust Centre Link Key (TCLK) for communication between the local node and the Trust Centre - the Trust Centre will respond with the requested link key
To request an application link key for communication with another node that is not the Trust Centre (in this case, the IEEE/MAC address of the other node must be supplied in the function call) - the Trust Centre will send the requested link key to both nodes
The Trust Centre will ignore the request if the node is not permitted to send APS secured data. The Trust Centre responses are encrypted as follows:
If a link key exists for communications between the Trust Centre and the target node (for example, a pre-configured link key), this key and the network key are both used to encrypt the requested link key.
Otherwise, only the network key is used to encrypt the requested link key.
On receiving the link key, the ZigBee stack on the node will automatically save the key. The event zps_EVENT_ZDO_LINK_KEY is generated to indicate that the link key is available. Any subsequent unicast or bound data transfer between these two nodes can opt to use this key (zps_E_APL_AF_SECURE_APL).
Note: An application link key can be introduced directly by the application using the function zps_eAplZdoAddReplaceLinkKey().
Note:
When a link key is used to encrypt a data packet, the packet payload is encrypted at the application level using the link key and then the packet is encrypted at the ZigBee stack NWK layer using the network key (therefore, both keys are used).
When application-level security is used in sending data, the IEEE/MAC address and network address of the target node must be available through the local Address Map table - see Section 6.2.3.
Parent topic:Setting up ZigBee security
Parent topic:Implementing ZigBee security