ZigBee Timer resources#
The ZigBee Timer functions are concerned with initializing and operating software timers. These resources are provided in the header file ZTimer.h.
The ZigBee Timer functions are described in Section 10.2.1
The ZigBee Timer structures are described in Section 10.2.2
ZigBee Timer functions#
The functions are listed below.
Function page#
To use the software timers, the while loop of your application must include a call to the following function:
void ZTIMER\_vTask\(void\);
Parent topic:ZigBee Timer functions
ZTIMER_eInit#
ZTIMER_teStatus ZTIMER_eInit(ZTIMER_tsTimer *psTimers,
uint8 u8NumTimers);
Description#
This function initializes a set of software timers for use by the application. A list of timers is provided in an array, in which each array element is a structure containing information on one timer (see Section 10.2.2.1). The index of an array element is used as a reference for the corresponding timer.
In order to use one of the initialized timers, it must first be opened using ZTIMER_eOpen().
Parent topic:ZTIMER_eInit
Parameters#
psTimers: Pointer to an array of structures, where each array element contains information for one timer (see Section 10.2.2.1)
u8NumTimers: Number of timers in the above array
Parent topic:ZTIMER_eInit
Returns#
E_ZTIMER_OK (timers successfully initialized)
E_ZTIMER_FAIL (timers not initialized)
Parent topic:ZTIMER_eInit
Parent topic:ZigBee Timer functions
ZTIMER_eOpen#
ZTIMER_teStatus ZTIMER_eOpen(
uint8 *pu8TimerIndex,
ZTIMER_tpfCallback pfCallback,
void *pvParams,
uint8 u8Flags);
Description#
This function is used to open the specified software timer. A list of parameter values for the timer must be provided as well as a user-defined callback function that will be used to perform any operations required on expiration of the timer.
The callback function has the following prototype:
typedef void (*ZTIMER_tpfCallback)(void * pvParam );
where pvParam is a pointer to the timer parameters.
The function also includes a parameter u8Flags, which specifies whether the timer should allow or prevent sleep. When activity checks are made to decide whether the device can enter sleep mode, the value of this flag determines if the (running) timer will stop the device from going to sleep.
Before a timer is opened, it must have been initialized in a call to ZTIMER_eInit().
Parent topic:ZTIMER_eOpen
Parameters#
pu8TimerIndex Pointer to location containing the index number of the timer in the list of timers initialized using ZTIMER_eInit()
pfCallback Pointer to the user-defined callback function for the timer
pvParams Pointer to a list of parameter values for the timer u8Flags Flag indicating whether the timer should allow or prevent sleep, one of:
ZTIMER_FLAG_ALLOW_SLEEP
ZTIMER_FLAG_PREVENT_SLEEP
Parent topic:ZTIMER_eOpen
Returns#
E_ZTIMER_OK (timer successfully opened)
E_ZTIMER_FAIL (timer not opened)
Parent topic:ZTIMER_eOpen
Parent topic:ZigBee Timer functions
ZTIMER_eClose#
ZTIMER_teStatus ZTIMER_eClose(uint8 u8TimerIndex);
Description#
This function is used to close the specified software timer when it is no longer needed. The timer must have been previously opened using ZTIMER_eOpen().
Parent topic:ZTIMER_eClose
Parameters#
u8TimerIndex: Index number of the timer in the list of timers initialized using ZTIMER_eInit().
Parent topic:ZTIMER_eClose
Returns#
E_ZTIMER_OK (timer successfully closed)
E_ZTIMER_FAIL (timer not closed - may be running or already closed)
Parent topic:ZTIMER_eClose
Parent topic:ZigBee Timer functions
ZTIMER_eStart#
ZTIMER_teStatus ZTIMER_eStart(uint8 u8TimerIndex,
uint32 u32Time);
Description#
This function is used to start the specified software timer. The length of time for which the timer will run must be specified in milliseconds.
Before a timer is started, it must have been opened using ZTIMER_eOpen(). Once started, the timer can be stopped (before it expires) using ZTIMER_eStop().
Parent topic:ZTIMER_eStart
Parameters#
pu8TimerIndex: Index number of the timer in the list of timers initialized using ZTIMER_eInit().
u32Time: The time, in milliseconds, for which the timer should run.
Parent topic:ZTIMER_eStart
Returns#
E_ZTIMER_OK (timer successfully started)
E_ZTIMER_FAIL (timer not started)
Parent topic:ZTIMER_eStart
Parent topic:ZigBee Timer functions
ZTIMER_eStop#
ZTIMER_teStatus ZTIMER_eStop(uint8 u8TimerIndex);
Description#
This function is used to stop the specified software timer (before it expires). The timer must have been previously started using ZTIMER_eStart().
Parent topic:ZTIMER_eStop
Parameters#
pu8TimerIndex: Index number of the timer in the list of timers initialized using ZTIMER_eInit().
Parent topic:ZTIMER_eStop
Returns#
E_ZTIMER_OK (timer successfully stopped)
E_ZTIMER_FAIL (timer not stopped - may be already stopped or expired)
Parent topic:ZTIMER_eStop
Parent topic:ZigBee Timer functions
ZTIMER_eGetState#
ZTIMER_teStatus ZTIMER_eGetState(uint8 u8TimerIndex);
Description#
This function is used to obtain the current state of the specified software timer. The possible reported states are:
Running
Stopped
Expired
Closed
Parent topic:ZTIMER_eGetState
Parameters#
pu8TimerIndex Index number of the timer in the list of timers initialized using ZTIMER_eInit().
Parent topic:ZTIMER_eGetState
Parent topic:ZigBee Timer functions
Parent topic:ZigBee Timer resources
ZigBee timer structures#
ZTIMER_tsTimer#
The ZigBee timer structure is shown below. It is used to represent a single software timer that may be used by the application.
typedef struct
{
ZTIMER_teState eState;
uint32 u32Time;
void *pvParameters;
ZTIMER_tpfCallback pfCallback;
} ZTIMER_tsTimer;
where:
eStaterepresents the current state of the timer, as one of:E_ZTIMER_STATE_CLOSED
E_ZTIMER_STATE_STOPPED
E_ZTIMER_STATE_RUNNING
E_ZTIMER_STATE_EXPIRED
u32Timeis the remaining time, in milliseconds, that the timer still has to runpvParametersis a pointer to a set of parameters used by the timerpfCallbackis a pointer to the user-defined callback function that will be called when the timer expires - this function has the prototype:typedef void \(\*ZTIMER\_tpfCallback\)\(void \pvParam*\);
where
pvParamis a pointer to the timer parameters.
Parent topic:ZigBee timer structures
Parent topic:ZigBee Timer resources
Parent topic:General ZPS Resources