MCUXpresso SDK Documentation

ZPS_eAplFormDistributedNetworkRouter

ZPS_eAplFormDistributedNetworkRouter#

ZPS_teStatus ZPS_eAplFormDistributedNetworkRouter(
        ZPS_tsAftsStartParamsDistributed *psStartParms,
        bool_t bSendDeviceAnnce);

Description#

This function can be used on a Router node to introduce the node into a distributed security network (see Section 6.10.2). The function must be called on the Router node that creates the distributed security network, therefore, the first node of the new network.

Subsequent Router nodes may be introduced using this function, but could be introduced using other commissioning methods, such as Touchlink.

Parent topic:ZPS_eAplFormDistributedNetworkRouter

Parameters#

  • psStartParms Pointer to structure containing the start parameter values for the Router- see Section 8.2.3.7.

  • bSendDeviceAnnce Boolean indicating whether a device announcement message is to be sent:

    • TRUE - send device announcement

    • FALSE - do not send device announcement

Parent topic:ZPS_eAplFormDistributedNetworkRouter

Returns#

Parent topic:ZPS_eAplFormDistributedNetworkRouter

Parent topic:initialization functions