MCUXpresso SDK Documentation

ZPS_eAplInitEndDeviceDistributed

ZPS_eAplInitEndDeviceDistributed#

ZPS_teStatus ZPS_eAplInitEndDeviceDistributed(
            ZPS_tsAftsStartParamsDistributed *psStartParms);

Description#

This function can be used on an End Device node to introduce the node into a distributed security network (see Section 6.10.2). This network must have already been created by a Router using the ZPS_eAplFormDistributedNetworkRouter() function. End Device nodes may be introduced into the network in this way or using other commissioning methods, such as Touchlink.

Parent topic:ZPS_eAplInitEndDeviceDistributed

Parameters#

psStartParms Pointer to structure containing the start parameter values for the End Device - see Section 8.2.3.7, ZPS_tsAftsStartParamsDistributed.

Parent topic:ZPS_eAplInitEndDeviceDistributed

Parent topic:ZPS_vAplAfEnableMcpsFilter

Returns#

Parent topic:ZPS_eAplInitEndDeviceDistributed

Parent topic:initialization functions