ZPS_eAplZdpBindRegisterRequest#
ZPS_teStatus ZPS_eAplZdpBindRegisterRequest(
PDUM_thAPduInstance hAPduInst,
ZPS_tuAddress uDstAddr,
bool bExtAddr,
uint8 *pu8SeqNumber,
ZPS_tsAplZdpBindRegisterReq *psZdpBindRegisterReq);
Description#
This function informs a remote node with a primary binding table cache that the local node will hold its own binding table entries (and therefore the remote node does not need to hold these entries). The function sends a Bind_Register_req request to the remote node.
The IEEE address of the local node must be specified in the request, which is represented by the structure below (further detailed in Section 8.2.2.25).
typedef struct {
uint64 u64NodeAddress;
} ZPS_tsAplZdpBindRegisterReq;
The remote node replies with a Bind_Register_rsp response, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpBindRegisterRsp(detailed in Section 9.2.3.25). This response contains any information stored about the binding on the remote.
Parent topic:ZPS_eAplZdpBindRegisterRequest
Parameters#
hAPduInst Handle of APDU instance in which request is sent.
uDstAddr Address of destination node of request (can be 16- or 64-bit, as specified by bExtAddr)
bExtAddr Type of destination address:
TRUE: 64-bit IEEE (MAC) address
FALSE: 16-bit network address
* pu8SeqNumber Pointer to sequence number of request
* psZdpPowerDescReq Pointer to request (see above)
Parent topic:ZPS_eAplZdpBindRegisterRequest
Returns#
ZPS_E_SUCCESS (request successfully sent)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdpBindRegisterRequest
Parent topic:Binding functions