MCUXpresso SDK Documentation

ZPS_eAplZdpExtendedActiveEpRequest

ZPS_eAplZdpExtendedActiveEpRequest#

ZPS_teStatus ZPS_eAplZdpExtendedActiveEpRequest(
    PDUM_thAPduInstance hAPduInst,
    ZPS_tuAddress uDstAddr,
    bool bExtAddr,
    uint8 *pu8SeqNumber,
    ZPS_tsAplZdpExtendedActiveEpReq
    *psZdpExtendedActiveEpReq);

Description#

This function requests a list of the active endpoints on a remote node. The function should be called if the node has more active endpoints than could be included in a response to ZPS_eAplZdpActiveEpRequest(). The function sends an Extended_Active_EP_req request either to the relevant node or to another node that may hold the required information in its primary discovery cache.

The network address of the node of interest must be specified in the request, which is represented by the structure below (further detailed in Section 9.2.2.12).

typedef struct { uint16 u16NwkAddr;

uint8 u8StartIndex;

} ZPS_tsAplZdpExtendedActiveEpReq;

This structure allows you to specify the first endpoint of interest for the request.

The endpoint list is received in an Extended_Active_EP_rsp response, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpExtendedActiveEpRsp(detailed in Section9.2.3.11).

Parent topic:ZPS_eAplZdpExtendedActiveEpRequest

Parameters#

  • hAPduInst Handle of APDU instance in which request is sent.

  • uDstAddr Address of destination node of request (can be 16- or 64-bit, as specified by bExtAddr)

  • bExtAddr Type of destination address:

    • TRUE: 64-bit IEEE (MAC) address

    • FALSE: 16-bit network address

  • * pu8SeqNumber Pointer to sequence number of request

  • * psZdpActiveEpReq Pointer to request (see above)

Parent topic:ZPS_eAplZdpExtendedActiveEpRequest

Returns#

  • ZPS_E_SUCCESS (request successfully sent)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdpExtendedActiveEpRequest

Parent topic:Service Discovery functions