MCUXpresso SDK Documentation

ZPS_eAplZdpRemoveBkupBindEntryRequest

ZPS_eAplZdpRemoveBkupBindEntryRequest#

ZPS_teStatus ZPS_eAplZdpRemoveBkupBindEntryRequest(
    PDUM_thAPduInstance hAPduInst,
    ZPS_tuAddress uDstAddr,
    bool bExtAddr,
    uint8 *pu8SeqNumber,
    ZPS_tsAplZdpRemoveBkupBindEntryReq
            *psZdpRemoveBkupBindEntryReq);

Description#

This function requests the removal of an entry in the back-up binding table cache on a remote node. The function must be called from the node with the corresponding primary binding table cache. The removal of a back-up entry is normally required when an entry in the primary binding table cache has been removed.

Note: This function is provided in the NXP ZDP API for the reason of interoperability with nodes running non-NXP ZigBee PRO stacks that support the generated request. On receiving a request from this function, the NXP ZigBee PRO stack will return the status ZPS_ZDP_NOT_SUPPORTED.

This request must include the binding table entry to be removed. The request is represented by the structure below (further detailed in Section 9.2.2.28).

typedef struct {

uint64 u64SrcAddress; uint8 u8SrcEndPoint; uint16 u16ClusterId; uint8 u8DstAddrMode; union {

struct {

uint16 u16DstAddress;

} sShort; struct {

uint64 u64DstAddress; uint8 u8DstEndPoint;

} sExtended;

};

} ZPS_tsAplZdpRemoveBkupBindEntryReq;

On receiving the request, the remote node removes the specified binding table entry from its back-up binding table cache, if possible.

The remote node replies with a Remove_Bkup_Bind_Entry_rsp response, which should be collected using the function **ZQ_bZQueueReceive()**and stored in a structure of type ZPS_tsAplZdpRemoveBkupBindEntryRsp(detailed in Section9.2.3.28).

Parent topic:ZPS_eAplZdpRemoveBkupBindEntryRequest

Parameters#

  • hAPduInst Handle of APDU instance in which request is sent.

  • uDstAddr Address of destination node of request (can be 16- or 64-bit, as specified by bExtAddr)

  • bExtAddr Type of destination address:

    • TRUE: 64-bit IEEE (MAC) address

    • FALSE: 16-bit network address

  • * pu8SeqNumber Pointer to sequence number of request

  • * psZdpRemoveBkupBindEntryReq Pointer to request (see above)

Parent topic:ZPS_eAplZdpRemoveBkupBindEntryRequest

Returns#

  • ZPS_E_SUCCESS (request successfully sent)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdpRemoveBkupBindEntryRequest

Parent topic:Binding functions