MCUXpresso SDK Documentation

ZPS_eAplZdpSimpleDescRequest

ZPS_eAplZdpSimpleDescRequest#

ZPS\_teStatus ZPS\_eAplZdpSimpleDescRequest\(
    PDUM\_thAPduInstance hAPduInst,
    ZPS\_tuAddress uDstAddr,
    bool bExtAddr,
    uint8 *pu8SeqNumber,
    ZPS\_tsAplZdpSimpleDescReq *psZdpSimpleDescReq);

Description#

This function requests the Simple descriptor for a specific endpoint on the node with a particular network address. The function sends a Simple_Desc_req request either to the relevant node or to another node that may hold the required information in its primary discovery cache.

The network address of the node of interest and the relevant endpoint on the node must be specified in the request, which is represented by the structure below (further detailed in Section 9.2.2.6).

typedef struct {

uint16 u16NwkAddrOfInterest; uint8 u8EndPoint;

} ZPS_tsAplZdpSimpleDescReq;

The required Simple descriptor is received in a Simple_Desc_rsp response, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpSimpleDescRsp(detailed in Section 9.2.3.5).

Parent topic:ZPS_eAplZdpSimpleDescRequest

Parameters#

  • hAPduInst: Handle of APDU instance in which request is sent

  • uDstAddr: Address of destination node of request (can be 16- or 64-bit, as specified by bExtAddr)

  • bExtAddr: Type of destination address:

    • TRUE: 64-bit IEEE (MAC) address

    • FALSE: 16-bit network address

  • *pu8SeqNumber: Pointer to sequence number of request

  • *psZdpSimpleDescReq: Pointer to request (see above).

Parent topic:ZPS_eAplZdpSimpleDescRequest

Returns#

  • ZPS_E_SUCCESS (request successfully sent)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdpSimpleDescRequest

Parent topic:Service Discovery functions