MCUXpresso SDK Documentation

ZPS_eAplZdpUserDescSetRequest

ZPS_eAplZdpUserDescSetRequest#

ZPS_teStatus ZPS_eAplZdpUserDescSetRequest(
    PDUM_thAPduInstance hAPduInst,
    ZPS_tuAddress uDstAddr,
    bool bExtAddr,
    uint8 *pu8SeqNumber,
    ZPS_tsAplZdpUserDescSet *psZdpUserDescSetReq);

Description#

This function can be used to configure the User descriptor on a remote node. The function sends a User_Desc_set request either to the remote node or to another node that may hold the relevant User descriptor in its primary discovery cache.

Note: This function can only be used to access the User descriptor of a non-NXP device (which supports this descriptor), since the storage of a User descriptor on an NXP device is not supported.

The network address of the node of interest as well as the required modifications must be specified in the request, which is represented by the structure below (further detailed in Section 9.2.2.13).

typedef struct {

uint16 u16NwkAddrOfInterest; uint8 u8Length;

char szUserDescriptor[ZPS_ZDP_LENGTH_OF_USER_DESC];

} ZPS_tsAplZdpUserDescSet;

If the specified User descriptor was successfully modified, a User_Desc_conf response is received. This response should be collected by the application task using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpUserDescConf(detailed in Section 9.2.3.12).

Parent topic:ZPS_eAplZdpUserDescSetRequest

Parameters#

  • hAPduInst Handle of APDU instance in which request is sent

  • uDstAddr Address of destination node of request (can be 16-bit or 64-bit, as specified by bExtAddr)

  • bExtAddr: Type of destination address:

    • TRUE: 64-bit IEEE (MAC) address

    • FALSE: 16-bit network address

  • *pu8SeqNumber: Pointer to sequence number of request

  • *psZdpUserDescSetReq: Pointer to request (see above)

Parent topic:ZPS_eAplZdpUserDescSetRequest

Returns#

  • ZPS_E_SUCCESS (request successfully sent)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdpUserDescSetRequest

Parent topic:Service Discovery functions