MCUXpresso SDK Documentation

ZPS_tsAplZdpNodeDescStoreReq

ZPS_tsAplZdpNodeDescStoreReq#

This structure is used by the function ZPS_eAplZdpNodeDescStoreRequest(). It represents a request to a remote node to store the Node descriptor of the local node.

The ZPS_tsAplZdpNodeDescStoreReqstructure is detailed below.

typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;

/* Rest of message is variable length */ ZPS_tsAplZdpNodeDescriptor sNodeDescriptor;

} ZPS_tsAplZdpNodeDescStoreReq;

where:

  • u16NwkAddris the network address of the sending node

  • u64IeeeAddris the IEEE address of the sending node

  • sNodeDescriptoris a pointer to the Node descriptor to store (this is itself a structure of the type ZPS_tsAplZdpNodeDescriptor, detailed in Section8.2.1.1)

Parent topic:ZDP Request structures