MCUXpresso SDK Documentation

tsOTA_ImageBlockResponsePayload

tsOTA_ImageBlockResponsePayload#

The following structure contains payload data for an Image Block Response issued by the server (as the result of an Image Block Request from a client):

typedef struct
{
            uint8 u8Status;
            union
            {
                         tsOTA_WaitForData                   sWaitForData;
         tsOTA_SuccessBlockResponsePayload   sBlockPayloadSuccess;
            }uMessage;
}tsOTA_ImageBlockResponsePayload;

where:

  • u8Status indicates whether a data block is included in the response:

    • OTA_STATUS_SUCCESS: A data block is included

    • OTA_STATUS_WAIT_FOR_DATA: No data block is included - client should re-request a data block after a waiting time

  • The element used from the union depends on the status reported above:

    • sWaitForData is a structure containing information used to instruct the requesting client to wait for a time before requesting the data block again or requesting the next data block (see Section 49.11.15) - this information is only provided in the case of the status OTA_STATUS_WAIT_FOR_DATA

    • sBlockPayloadSuccess is a structure containing a requested data block and associated information (see Section 49.11.13) - this data is only provided in the case of the status OTA_STATUS_SUCCESS

Parent topic:Structures