tsOTA_SuccessBlockResponsePayload#
The following structure contains payload data for an Image Block Response which reports ‘success’ and therefore contains a block of image data (see Section 49.11.10):
typedef struct
{
uint8* pu8Data;
uint32 u32FileOffset;
uint32 u32FileVersion;
uint16 u16ImageType;
uint16 u16ManufacturerCode;
uint8 u8DataSize;
}tsOTA_SuccessBlockResponsePayload;
where:
pu8Datais a pointer to the start of the data block being transferredu32FileOffsetis the offset, in bytes, of the start of the data block from the start of the image (normally, the same offset as specified in the Image Block Request)u32FileVersionis the file version of the upgrade image to which the included data block belongsu16ImageTypeis the type of the upgrade image to which the included data block belongsu16ManufacturerCodeis the manufacturer code that was received from the client in the Image Block Requestu8DataSizeis the length, in bytes, of the included data block (this must be less than or equal to the maximum data block length for the client, specified in the Image Block Request)
Parent topic:Structures