vOTA_GenerateHash#
void vOTA_GenerateHash(
tsZCL_EndPointDefinition *psEndPointDefinition,
tsOTA_Common *psCustomData,
bool bIsServer,
bool bHeaderPresent,
AESSW_Block_u *puHash,
uint8 u8ImageLocation);
Description#
This function can be used to generate a hash checksum for an application image in Flash memory, using the Matyas-Meyer-Oseas cryptographic hash.
Parameters#
psEndPointDefinition Pointer to structure which defines endpoint corresponding to the application (see Section 6.1.1)
psCustomData Pointer to data structure connected with event associated with the checksum (see Section 49.11.2)
bIsServer Side of cluster implemented on this device:
TRUE - Server
FALSE - Client
bHeaderPresent Presence of image header:
TRUE - Present
FALSE - Absent
puHash Pointer to structure to receive calculated hash checksum
u8ImageLocation Number of sector where image starts in Flash memory
Returns#
None
Parent topic:General Functions