Hardware requirements
Micro USB cable
MCIMX7ULP-EVK board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Please note that this application must be built with flash link file! Build with RAM link file might fail due to shortage of RAM size.
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW1 to power on the board.
Connect a micro USB cable between the host PC and the J6 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
The log below shows the output of the mbedtls_selftest example in the terminal window:
mbedTLS version 2.13.1
fsys=115200000
Using following implementations:
SHA: MMCAU HW accelerated
AES: LTC HW accelerated
AES GCM: MMCAU HW accelerated
DES: MMCAU HW accelerated
Asymmetric encryption: Software implementation
MD5 test #1: passed
MD5 test #2: passed
MD5 test #3: passed
MD5 test #4: passed
MD5 test #5: passed
MD5 test #6: passed
MD5 test #7: passed
SHA-1 test #1: passed
SHA-1 test #2: passed
SHA-1 test #3: passed
SHA-224 test #1: passed
SHA-224 test #2: passed
SHA-224 test #3: passed
SHA-256 test #1: passed
SHA-256 test #2: passed
SHA-256 test #3: passed
SHA-384 test #1: passed
SHA-384 test #2: passed
SHA-384 test #3: passed
SHA-512 test #1: passed
SHA-512 test #2: passed
SHA-512 test #3: passed
DES -ECB- 56 (dec): passed
DES -ECB- 56 (enc): passed
DES3-ECB-112 (dec): passed
DES3-ECB-112 (enc): passed
DES3-ECB-168 (dec): passed
DES3-ECB-168 (enc): passed
DES -CBC- 56 (dec): passed
DES -CBC- 56 (enc): passed
DES3-CBC-112 (dec): passed
DES3-CBC-112 (enc): passed
DES3-CBC-168 (dec): passed
DES3-CBC-168 (enc): passed
AES-ECB-128 (dec): passed
AES-ECB-128 (enc): passed
AES-ECB-192 (dec): skipped
AES-ECB-192 (enc): skipped
AES-ECB-256 (dec): skipped
AES-ECB-256 (enc): skipped
AES-CBC-128 (dec): passed
AES-CBC-128 (enc): passed
AES-CBC-192 (dec): skipped
AES-CBC-192 (enc): skipped
AES-CBC-256 (dec): skipped
AES-CBC-256 (enc): skipped
AES-CFB128-128 (dec): passed
AES-CFB128-128 (enc): passed
AES-CFB128-192 (dec): skipped
AES-CFB128-192 (enc): skipped
AES-CFB128-256 (dec): skipped
AES-CFB128-256 (enc): skipped
AES-CTR-128 (dec): passed
AES-CTR-128 (enc): passed
AES-CTR-128 (dec): passed
AES-CTR-128 (enc): passed
AES-CTR-128 (dec): passed
AES-CTR-128 (enc): passed
AES-GCM-128 #0 (enc): passed
AES-GCM-128 #0 (dec): passed
AES-GCM-128 #0 split (enc): passed
AES-GCM-128 #0 split (dec): passed
AES-GCM-128 #1 (enc): passed
AES-GCM-128 #1 (dec): passed
AES-GCM-128 #1 split (enc): passed
AES-GCM-128 #1 split (dec): passed
AES-GCM-128 #2 (enc): passed
AES-GCM-128 #2 (dec): passed
AES-GCM-128 #2 split (enc): passed
AES-GCM-128 #2 split (dec): passed
AES-GCM-128 #3 (enc): passed
AES-GCM-128 #3 (dec): passed
AES-GCM-128 #3 split (enc): passed
AES-GCM-128 #3 split (dec): passed
AES-GCM-128 #4 (enc): passed
AES-GCM-128 #4 (dec): passed
AES-GCM-128 #4 split (enc): passed
AES-GCM-128 #4 split (dec): passed
AES-GCM-128 #5 (enc): passed
AES-GCM-128 #5 (dec): passed
AES-GCM-128 #5 split (enc): passed
AES-GCM-128 #5 split (dec): passed
CCM-AES #1: passed
CCM-AES #2: passed
CCM-AES #3: passed
Base64 encoding test: passed
Base64 decoding test: passed
MPI test #1 (mul_mpi): passed
MPI test #2 (div_mpi): passed
MPI test #3 (exp_mod): passed
MPI test #4 (inv_mod): passed
MPI test #5 (simple gcd): passed
RSA parse key #1 : passed
RSA-1024 key validation: passed
PKCS#1 encryption : passed
PKCS#1 decryption : passed
PKCS#1 data sign : passed
PKCS#1 sig. verify : passed
X.509 certificate load: passed
X.509 signature verify: passed
HMAC_DRBG (PR = True) : passed
HMAC_DRBG (PR = False) : passed
ECP test #1 (constant op_count, base point G): passed
ECP test #2 (constant op_count, other point): passed
DHM parameter load: passed
ENTROPY test: passed
PBKDF2 (SHA1) #0: passed
PBKDF2 (SHA1) #1: passed
PBKDF2 (SHA1) #2: passed
PBKDF2 (SHA1) #3: passed
PBKDF2 (SHA1) #4: passed
PBKDF2 (SHA1) #5: passed
Executed 17 test suites
[ All tests PASS ]