Hardware requirements#
Mini/micro USB cable
EVK-MIMXRT1020 board
Personal Computer
Headphone
Board settings#
Please insert the SDCARD into card slot(J15), make sure C28 is welded.
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Insert the headphones into the headphone jack on EVK-MIMXRT1020 board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
This following section shows how to run the demo: Notice, on EVK-MIMXRT1020 board, the audio record source is from two microphones. The left channel is from the headphone microphone, the right channel from the main microphone on board. It is OK for you to choose one of them or both. As the headphone microphone may have headphone standard differernt issue, you can just use main microphone on board as input source.
Please note that the log print out may be different according to the different card, If the card doesn’t been formatted ,the case will making new file system and below log will be printed,
SAI Peripheral Demo started!
Please insert a card into board.
Card inserted.
Make file system......The time may be long if the card capacity is big.
Create directory......
Please choose the option :
1. Record and playback at same time
2. Playback sine wave
3. Record to SDcard, after record playback it
4. Quit
If the card is formatted already, the case will mount the file system only, the case will print below log,
SAI Peripheral Demo started!
Please insert a card into board.
Card inserted.
Mount volume Successfully.
Create directory......
Please choose the option :
1. Record and playback at same time
2. Playback sine wave
3. Record to SDcard, after record playback it
4. Quit
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.