Hardware requirements
- Micro USB cable 
- EVK-MIMXRT595 REV C1 board 
- Personal Computer 
Board settings
Make sure resistors R691~R697 are removed and resistors R611~R620,R660,R661,R698 are populated.
Prepare the Demo
- Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board 
- Open a serial terminal with the following settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Launch the debugger in your IDE to begin running the demo. 
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
MMCCARD freertos example.
Read/write the card continuously until encounter error......
Write/read one data block......
Compare the read/write content......
The read/write content is consistent.
Write/read multiple data blocks......
Compare the read/write content......
The read/write content is consistent.
Erase data groups......
Input 'q' to quit read/write/erase process.
Input other char to read/write/erase data blocks again.