Hardware requirements
- Mini/micro USB cable 
- MCX-N9XX-EVK board 
- Personal Computer 
Board settings
Prepare the Demo
- Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board 
- Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number): - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.