MCUXpresso SDK Documentation

digital_connected_cluster

digital_connected_cluster#

Overview#

This example demo is for demonstrating multiple Bluetooth profiles tailored to two-wheeler use case scenarios, enabling below features for enhanced rider experience.

Where device is connected to Rider Mobile, Rider Headset and Passenger Headset.

  1. A2DP audio bridging : Phone music is played to Rider Headset. Device receives the audio streaming data and forwards to Rider Headset.

  2. eSCO bridge (HFP call bridging) : Phone call audio is routed to Rider Headset. User can answer\reject call from Rider headset or using shell command. Once eSCO connection with Phone and Rider Headset established the IW611\IW612 controller will forward eSCO Audio packets from Phone to Rider Headset & vice versa.

  3. DUAL A2DP : Play local default music or music from USB drive to both Rider and Passenger Headset.

  4. Intercom : With this feature Rider and Passenger will able to communicate each other. User can end intercom with shell command or end call from Headset.

  5. PBAP and MAP : Phone contact download using PBAP profile, regeter & receive message notification.

Prepare the Demo#

  1. Open example’s project and build it.

  2. Connect a USB cable between the PC host and the OpenSDA USB port on the target board.

  3. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo#

The log below shows the output of the example in the terminal window.

Note:

  1. Please use the command “help” to view the specific commands supported by the example.

  2. The shell information “SHELL build: Aug 10 2021” may be different, which depends on the compile date.

  3. For MAP and PBAP with iOS, need to allow contact sync and message notification from Bluetooth settings.

  4. When running example first time, make sure to delete existing all paired devices. bt delete_all

DIGITAL CONNECTED CLUSTER Demo started....
download starts(400568)
........................................................................................................................
download success!
Bluetooth initialized
Copyright  2024  NXP
>>

The suppprted command details are as follows : “bt”: BT related function

USAGE: bt [discover|connect|disconnect|delete_all|paired_list]

discover             to find Bluetooth devices

connect <device_index>
                     connect to the device that is found in discovery,

                     bt connect <device index> index is device index from discovery list displayed

					 bt connect <device index>             // Connect to Rider Headset or Mobile.
                     bt connect <device index>  PH/ph     // Connect to Passenger Headset. 
					    
connect_paired  <device_index>

                     The <device index> is from paired device list displayed 
					 
disconnect           disconnect Bluetooth link

                     bt disconnect <device type>

                     For example:

                     bt disconnect M/m -> for Rider mobile device disconnection

                     bt disconnect H/h -> for Rider headset disconnection

                     bt disconnect PH/ph -> for Passenger headset disconnection

delete_all           delete all devices. The device is connected then it will be disconnected.

delete_dev <index>   To delete particular device from paired list

paired_list          Get the paired devices

set_hstype           bt set_hstype <index> <type>                        
						index - index from paired list                        
						type ph - set as passenger headset                        
						type h - set as rider headset

“bt”: AVRCP related function

USAGE: bt [play|pause|volume up|volume down|next|previous]

play                 to play the song

pause                to pause the song for

volume up            increase the volume

volume down          decrease the volume

next                 goto the next song

previous             goto the previous song

get_song_detail      get current playing song details   

hs_play<option>      to start music in DUAL A2DP mode                        
						h: start play with rider headset 
						ph: with passenger headset  
					 
hs_stop<option>      to stop music in DUAL A2DP mode            
						h: stop play with rider headset   
						ph: with passenger headset

“bt”: HFP related function

USAGE: bt [dial|aincall|eincall]

dial                 dial out call.

hf_aincall           accept the incoming call.

hf_eincall <index>   index 0: call decline w/o msg 1: with msg  end an incoming call.

clcc                 Query list of current calls.

micVolume            Update mic Volume.

speakerVolume        Update Speaker Volume.

lastdial             call the last dialed number.

“bt”: PBAP related function

USAGE: bt [get_pbap_data | contact_list ]

get_pbap_data <option>  0:All contacts 1:Missed calls 2:Incoming 3:Outgoing

contact_list 0           show downloaded contact list

“bt”: MAP related function

USAGE: bt reg_msg_ntf Register for message notification

USAGE: bt show_messages To show the available default messages rider wants to set

USAGE: bt set_message To set the default rejet call message.

USAGE: bt get_message To get the messages from connected mobile

USAGE: bt send_message To send the message from the connected mobile

“bt”: A2DP bridge|DUAL A2DP mode functions

USAGE: bt a2dp_mode

1.Device pair, connect and disconnection •bt discover – Start Bluetooth discovery to find nearby devices. •bt connect – Connect to the discovered device at the specified index. Example: bt connect 1 (1 is index from discover list) •The headset by default identified as Rider Headset, to mark it as passenger headset use additional argument “ph” Example: bt connect 1 ph (1 is index from discover list, ph for passenger headset) •bt disconnect <M(m)/H(h)/PH()ph> - Disconnect the Rider mobile, Rider headset and Passenger Headset

2.Connecting Paired Devices •If a device is already paired, then can connect using pair list index. Example: bt paired_list – Retrieve the list of paired devices. •bt connect_paired – Connect to a device from the paired list. Example: bt connect_paired 1 (Connects to the first device from paired list)

3.Deleting Paired Devices •bt delete_dev – Delete a specific paired device. Example: bt delete_dev 1 (Deletes the first paired device) •bt delete_all – Remove all paired devices.(Please note, if any connection exists, will be disconnected when deleting pairing)

4.Change Headset type Following command can be used to change headset type i.e. from Rider headset to Passenger headset or Passenger headset to Rider headset •bt set_hstype : where index is - index from paired list - type PH/ph - set as passenger headset - type H/h - set as rider headset

5.Running A2DP Bridge After connecting the mobile phone and headset, the user can play music from the mobile to headset, and control music play\pause and other operations via command line or few of the operations from headset directly i.e. play\pause, next\prev. Before using below operations, make sure a2dp_mode is set to 0. •bt a2dp_mode 0 // Enable a2dp bridge, •bt play – Play the song. •bt pause – Pause the song. •bt volume up – Increase the volume. •bt volume down – Decrease the volume. •bt next – Skip to the next song. •bt previous – Go to the previous song. •bt get_song_detail – Retrieve details of the currently playing song.
•bt browse_getfolderitems - retrieve list of songs

6.Running SCO Bridge If an incoming call is received, the DUT displays the caller’s name and number and can answer\reject call using cli command or from headset. The user can manage calls using the following commands: Making & Receiving Calls •bt dial <mobile_num> – Dial an outgoing call. Example: bt dial 9876543210 •bt hf_aincall – Accept an incoming call. •bt hf_eincall

7.Running Dual A2DP Streaming Create connection to Rider Headset and Passenger Headset, after connection is success send below command to start music streaming to both headset . •bt a2dp_mode 2 - This will play default music to both headset. •bt a2dp_mode 1 - This will play song from USB drive, the song should be 44.1Khz wave file with name “dcc_test.wav” •bt a2dp_mode 0 - Initiate play from phone or headset to start music from Phone.

	In DUAL mode enabled, play/stop individual headsets
		•bt hs_play   <option>  h: start play with rider headset, ph: with passenger headset
		•bt hs_stop   <option>  h: stop play with rider headset, ph: with passenger headset
	Notes - By default, the phone music (A2DP bridge mode) is enabled. The DUAL A2DP is paused when intercom is started and if can’t be resumed until intercom is disconnected. 

8.Running Intercom Feature Create connection to Rider Headset and Passenger Headset, after connection is success send below command to start intercom between headsets. •bt intercom 1 - To enable intercom •bt intercom 0 - To disconnect intercom. Like normal call if call end button press on headset will end the ongoing intercom session.
If there is incoming\outgoing call then intercom will get disconnected and will be resumed once phone call is ended.

  1. Running PBAP Functions When connecting to phone the PBAP connection is initiated automatically. To fetch phonebook contacts\missed call\incoming\outgoing calls can use below command •bt get_pbap_data 0 – download phonebook contacts. •bt get_pbap_data 1 - get missed call list •bt get_pbap_data 2 - get incoming call list •bt get_pbap_data 3 - get outgoing call list

  2. Running the MAP functions. When connecting to phone the MAP connection is initiated automatically. •bt reg_msg_ntf - After registration, new messages will be fetched and showed on terminal. •bt show_messages - To show the available messages rider wants to set during rejecting the call. •bt set_message - To set the pre-defined message from the list, which will be sent when rejecting call with message. •bt get_message - To get the messages from connected mobile. •bt send_message - To send the message from the connected mobile.

Supported Boards#