tflm_cifar10#
Overview#
Convolutional neural network (CNN) example with the use of convolution, ReLU activation, pooling and fully-connected functions.
The CNN model in the example was trained using the scripts available at [1] with the CifarNet model. The configuration of the model was modified to match the neural network structure in the CMSIS-NN CIFAR-10 example. The example source code is a modified version of the Label Image example from the TensorFlow Lite examples [2], adjusted to run on MCUs. The neural network consists of 3 convolution layers interspersed by ReLU activation and max pooling layers, followed by a fully-connected layer at the end. The input to the network is a 32x32 pixel color image, which is classified into one of the 10 output classes. The model size is 91 KB.
Firstly a static ship image is used as input regardless camera is connected or not. Secondly runtime image processing from camera in the case camera and display is connected. Camera data are displayed on LCD.
HOW TO USE THE APPLICATION: To classify an image, place an image in front of the camera so that it fits in the white rectangle in the middle of the LCD display. Note that semihosting implementation causes slower or discontinuous video experience. Select UART in ‘Project Options’ during project import for using external debug console via UART (virtual COM port).
[1] https://github.com/tensorflow/models/tree/master/research/slim [2] https://github.com/tensorflow/tensorflow/tree/r2.3/tensorflow/lite/examples/label_image
Files: main.cpp - example main function ship.bmp - shrinked picture of the object to recognize (source: https://en.wikipedia.org/wiki/File:Christian_Radich_aft_foto_Ulrich_Grun.jpg) image_data.h - image file converted to a C language array of RGB values using Python with the OpenCV and Numpy packages: import cv2 import numpy as np img = cv2.imread(‘ship.bmp’) img = cv2.cvtColor(img, cv2.COLOR_BGR2RGB) with open(‘image_data.h’, ‘w’) as fout: print(‘#define STATIC_IMAGE_NAME “ship”’, file=fout) print(‘static const uint8_t image_data[] = {’, file=fout) img.tofile(fout, ‘, ‘, ‘0x%02X’) print(‘};\n’, file=fout) timer.c - timer source code image/* - image capture and pre-processing code model/get_top_n.cpp - top results retrieval model/model_data.h - model data converted from a .tflite file to a C language array using the xxd tool (distributed with the Vim editor at www.vim.org) model/model.cpp - model initialization and inference code model/model_cifarnet_ops.cpp - model operations registration model/output_postproc.cpp - model output processing video/* - camera and display handling
This example cannot be imported into Config Tools because the xtensa toolchain is not supported.
Running the demo#
The log below shows the output of the demo in the terminal window (compiled with ARM GCC):
CIFAR-10 object recognition example using a TensorFlow Lite model. Detection threshold: 60% Expected category: ship Model: cifarnet_quant
Static data processing:#
Inference time: 65 ms
Detected: ship (100%)
Camera data processing: Data for inference are ready#
Inference time: 64 ms
Detected: dog (95%)
Data for inference are ready#
Inference time: 65 ms
Detected: No label detected (0%)
Data for inference are ready#
Inference time: 64 ms
Detected: horse (60%)
Supported Boards#
[EVK-MIMXRT595]