USB_DeviceGetStringDescriptor
This function is used to get the string descriptor. All devices must implement this function.
/* Get device string descriptor request */
usb_status_t USB_DeviceGetStringDescriptor(usb_device_handle handle,
usb_device_get_string_descriptor_struct_t *stringDescriptor)
{
if (stringDescriptor->stringIndex == 0U)
{
stringDescriptor->buffer = (uint8_t *)g_UsbDeviceLanguageList.languageString;
stringDescriptor->length = g_UsbDeviceLanguageList.stringLength;
}
else
{
uint8_t languageId = 0U;
uint8_t languageIndex = USB_DEVICE_STRING_COUNT;
for (; languageId < USB_DEVICE_STRING_COUNT; languageId++)
{
if (stringDescriptor->languageId == g_UsbDeviceLanguageList.languageList[languageId].languageId)
{
if (stringDescriptor->stringIndex < USB_DEVICE_STRING_COUNT)
{
languageIndex = stringDescriptor->stringIndex;
}
break;
}
}
if (USB_DEVICE_STRING_COUNT == languageIndex)
{
return kStatus_USB_InvalidRequest;
}
stringDescriptor->buffer = (uint8_t *)g_UsbDeviceLanguageList.languageList[languageId].string[languageIndex];
stringDescriptor->length = g_UsbDeviceLanguageList.languageList[languageId].length[languageIndex];
}
return kStatus_USB_Success;
}
Parent topic:USB descriptor functions
Parent topic:USB composite device descriptor examples