Compiler/Debugger

The MCUXpresso SDK i.MX 93 release supports building and debugging with the toolchains listed in Table 1.

The user can choose the appropriate one for development.

For supported toolchain versions, see MCUXpresso SDK Release Notes for MCIMX93AUTO-EVK (document: MCUXSDKMCIMX93AEVKRN).

  • Arm GCC + SEGGER J-Link GDB Server. This is a command line tool option and it supports both Windows OS and Linux OS.

  • IAR Embedded Workbench for Arm and SEGGER J-Link software. The IAR Embedded Workbench is an IDE integrated with editor, compiler, debugger, and other components. The SEGGER J-Link software provides the driver for the J-Link Plus debugger probe and supports the device to attach, debug, and download.

Compiler/Debugger

Supported host OS

Debug probe

Tool website

ArmGCC/J-Link GDB server

Windows OS/Linux OS

J-Link Plus

developer.arm.com/open-source/gnu-toolchain/gnu-rm

www.segger.com

| |IAR/J-Link|Windows OS|J-Link Plus|www.iar.com

www.segger.com

|

Download the corresponding tools for the specific host OS from the website.

Note:

Parent topic:Toolchain introduction