Hardware requirements#
Mini/micro USB cable
MIMXRT1060-EVKB board
Personal Computer
Headphone(OMTP standard)
CS42448 Audio board(Not necessary if use on board codec)
Board settings#
For Audio board: 1.Insert AUDIO board into J23 if on board codec is not used 2.Uninstall J41 For on board codec: 2.Make sure J41 is installed
Prepare the Demo#
Note: As the EVKBMIMXRT1060 support two codecs, a default on board WM8960 codec and another codec CS42448 on audio board, so to support both of the codecs, the example provide options to switch between the two codecs,
DEMO_CODEC_WM8960, set to 1 if wm8960 used
DEMO_CODEC_CS42448, set to 1 if cs42448 used Please do not set above macros to 1 together, as the demo support one codec only.
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board. Steps for WM8960:
Insert the headphones into the headphone jack on MIMXRT1060-EVKB board (J34). Steps for CS42448:
Insert the headphones into the headphone jack J6 on the audio board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
Note: This demo outputs 1000HZ sine wave audio signal. When the demo runs successfully, you can hear the tone and the log would be seen on the OpenSDA terminal like:
SAI functional interrupt example started!
SAI functional interrupt example finished!