Hardware requirements

  • Micro USB cable

  • MIMX8MN6-EVK board

  • J-Link Debug Probe

  • 12V power supply

  • Personal Computer

Board settings

No special settings are required.

Please note this application can’t support running with Uboot! and accordingly it does not support Flash target and DDR target! This example aims to show the basic usage of the IP’s function, some of the used Resources are assigned to Cortex-A core by uboot.

Prepare the Demo

  1. Connect 12V power supply and J-Link Debug Probe to the board, switch SW101 to power on the board

  2. Connect a USB cable between the host PC and the J901 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below is shown in the terminal window:

RDC Example:
RDC Peripheral access control
RDC Peripheral access control with SEMA42
RDC memory region access control

RDC Example Success