Hardware requirements
- Micro USB cable 
- MIMX8MN6-EVK board 
- J-Link Debug Probe 
- 12V power supply 
- Personal Computer 
Board settings
Connect input signal to J1001-43 Test Point.
Prepare the Demo
- Connect 12V power supply and J-Link Debug Probe to the board, switch SW101 to power on the board 
- Connect a USB cable between the host PC and the J901 USB port on the target board. 
- Open a serial terminal with the following settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Launch the debugger in your IDE to begin running the demo. 
Running the demo
When the example runs successfully, following information can be seen on the terminal:
GPT input capture example
Once the input signal is received the input capture value is printed